Part Number: UC1825A What is the value of the UC1825A under-voltage lockout (UVLO) start threshold voltage temperature coefficient? The datasheet lists a range of 8.4 to 9.6 volts over the full temperature range including initial tolerance, but does not…
Part Number: UC1825A-SP Other Parts Discussed in Thread: TINA-TI , UC1825A , Tool/software: TINA-TI or Spice Models Is there any device accurate model of UC1825A or UC1825A-SP supported in TINA-TI simulation tool? Don't see it in the standard library. If…
Part Number: UC1825A -Parts exhibit Extremely LOW or NO OUTPUT
**Please advise how much (%) solder connection is required for proper function on these parts
(Some integrated circuits require at least 70% solder contact with PCB to Leads) Please advise…
Other Parts Discussed in Thread: UC1825A , UC1825 , UC1825A-SP Hi,
UC1825 and UC1825A has below functions.
UC1825: Dual Totem Pole Outputs (Alternating) - Duty Cycle Range (%80max) - Dead-Time Control by Ct pin.
UC1825A: Dual Totem Pole Outputs (Alternating…
Other Parts Discussed in Thread: UC1825A do you have any design tools for UC1825a use like a spreadsheet for slope compensation, eff calcs, power diss., etc.
Raveej, I don't work for TI, I'm a user that had some of the issues you're having on a design last year. In particular, the problem of high minimum duty cycle. I worked with the TI engineer for almost 4-months before they concluded that there was no way…
Other Parts Discussed in Thread: UC1825A , UC1825 I'm using the TI UC1825AL PWM Control IC in a MIL/Hi-REL DC-DC Converter design. I'm an expert power electronics engineer, but never used the UC1825A before. The only documentation is the datasheet and an…
Hey Joe,
The UC1825B-SP is based on the UC1825-SP not the UC1825A-SP.
That's why the specification is not there for the UC1825B-SP.
Since its not tested I don't have any information on the EOL tolerances.
Thanks,
Daniel
Hi,
In our system, we must use NI pin with voltage level between 0V to 600 mV. Besides that, we are using UC1823A-SP so space products are essential for us. Therefore, some questions are:
1-) Is there same problem for NI pin in UC1825A-SP ?
2-) Are there…