Part Number: UC1825-SP Other Parts Discussed in Thread: UC1825 , UC1825A , UC1825B-SP , UC1825A-SP Hello,
I would like to know the SEE sensitivity of the UC1825-SP part.
I found two SEE radiation reports for the UC1825 family :
ESA_QCA0417S_C…
Hey Joe,
The UC1825B-SP is based on the UC1825-SP not the UC1825A-SP.
That's why the specification is not there for the UC1825B-SP.
Since its not tested I don't have any information on the EOL tolerances.
Thanks,
Daniel
Hi,
In our system, we must use NI pin with voltage level between 0V to 600 mV. Besides that, we are using UC1823A-SP so space products are essential for us. Therefore, some questions are:
1-) Is there same problem for NI pin in UC1825A-SP ?
2…
gG,
Can you look at UC1825a-sp and see if E/A and current feedback will do the trick. Alternately use an external op-amp i.e. LMP2012QML-SP in conjunction with UC1825A-SP. you can always put the internal op-amp in unity feedback and use external op…
Hi Francois,
TPS40200-EP is enhanced version of commercial part. I.e. TPS40200-EP is characterized over wider temp range -55C to 125C as opposed to the commercial part ( -40C to 125C).
You should look for xxx-SP parts i.e. UC1825A-SP , UC1843-SP…
Hi Ramesh,
Can you tell me the criteria apart from Duty cycle limit for a dual output controller to be used in an active clamp application?
UC1825A-SP has a duty cycle up to 85%. If duty cycle is the limiting factor to be used for the active clamp…
Other Parts Discussed in Thread: UC1825A , UC1825 , UC1825A-SP Hi,
UC1825 and UC1825A has below functions.
UC1825: Dual Totem Pole Outputs (Alternating) - Duty Cycle Range (%80max) - Dead-Time Control by Ct pin.
UC1825A: Dual Totem Pole Outputs…
Other Parts Discussed in Thread: MKT-WG16A-MS , MKT-WG10A-MS , SN0020HKH , SN0010HKU , TPS7H1111-SP , TPS7H4011-SP , TPS7H6003-SP , SN00020FK Looking for mechanical package samples for trim and form setup
Answer:
For our Space Power Ceramic QMLV qualified…