Part Number: UC1834-SP Other Parts Discussed in Thread: UC1846-SP , UC1834 , Tool/software: Thermal resistance for UC1834, LCC-20 package is not explicitly mentioned in the datasheet. I was referring to equivalent packaged UC1846-SP device which states…
Part Number: UC1834-SP Tool/software: During testing Vin pin has accidentally seen voltage greater than 40V, (0 to 80V in 40ms, then 80V to 40V in 40ms, approx 100ms IC has seen voltage greater than 40V)
After this although IC is working fine now, Can…
Part Number: UC1834 Please tell me the maximum voltage of the fault delay pin.
Question to determine the withstand voltage of a capacitor in an external circuit.
Part Number: UC1834-SP Hi,
The LCC package for UC1834-SP has multiple NC pins. Are these pins connected to the die in any way? Asking this if these can be connected to the thermal plane for better thermal performance
Thanks
Nandha
Part Number: UC1834-SP Other Parts Discussed in Thread: UC1901-SP , UC1834 Hi,
The datasheet does not specify the leakage current of the open collector output. Can I get a rough estimate for the worst case value for the leakage current over temperature…
Hey Meet,
The final picture in the datasheet shows a basic schematic of what it would look like.
A simple resistor divider on the output would do for the under voltage.
This will only set the fault alert pin, and you will have to implement external…
Part Number: UC1834 Hi,
Trying to juice out all I can from this IC (quite versatile I would say with an integrated reference and high current capacity compared to a standard opamp). The intended application is to use the IC to generate 0-100V, 5mA supply…
Part Number: UC1834-SP Other Parts Discussed in Thread: UC1834 Hi
Vin max is given as 36V at UC1834 webpage, whereas Absolute maximum as 40V in datasheet.
It is clear that there is no guarantee for functioning of IC above 40V, but what will be the…
Part Number: UC1834-SP Hello,
We are using this part in a design, and want to understand if any of the NC terminals needed to be grounded?
Thanks, Adam
Part Number: UC1834 Other Parts Discussed in Thread: UC2832-EP , UC3834 , UC2834 Hi I need to get the alternative part for the UC1834. Its a positive/negative regulator. Since UC1834 is costly I need to get a alternative part to test it. Can u suggest…