Part Number: UC1843A-SP Other Parts Discussed in Thread: UC1843-SP , UC1843 I am planning to use the UC1843A-SP in a non-SMPS function where the frequency will be low, between 10Hz and 300Hz. Also, I need to stop the oscillator in the position where the…
Other Parts Discussed in Thread: UC1843A-SP My customer would like to know if there are >100 or <100 transistors in the dies for the UC1843A-SP and TPS50601-RHA . He needs to know for reliability predictions.
Please let me know and thanks for your…
Part Number: UC1901-SP Other Parts Discussed in Thread: TIDA-070002 , UC1843A-SP , Team,
My immediate need is to come up with an architecture for a HARD Isolated House-Keeping power supply (~50W).
Similar to TIDA-070002
The PWM Controller’s (UC1843A-SP…
Part Number: UC1843-SP Other Parts Discussed in Thread: UC1843A , UC1843 Can provide the differences in die construction for 5962-8670402VXA, UC1843AMDREP and the 5962-8670409VPA? I would like to understand if the similarities and differences of the dies…
Other Parts Discussed in Thread: MKT-WG16A-MS , MKT-WG10A-MS , SN0020HKH , SN0010HKU , SN00020FK Looking for mechanical package samples for trim and form setup
Answer:
For our Power Ceramic QMLV qualified portfolio of devices we do offer the following mechanical…
Hey Sreenivasarao,
For applications with Vin <= 7 V I suggest the TPS50601A-SP
For applications with Vin > 7 V I suggest the UC1843A-SP.
If you are unable to use two different ones, the UC1843A-SP will likey have to work for the application.
Thanks…
Hey Ashley,
We have a UC1843B-SP coming out that will be similar to the UC1843A-SP but with higher radiation performance. You will need a discrete high side driver, but you would need one for the UC1846-SP anyway. The Abs max of the UC1843A-SP is 30…
Hey Josh,
You have quite a few topologies to choose from then. Do you have a low current requirement?
One of the more popular choices is a flyback with the UC1843A-SP controller. This is better for lower currents.
Thanks,
Daniel
Part Number: UC1845A-SP Other Parts Discussed in Thread: UC1845A , UC1845 , UC1843A-SP , UC1843A Tool/software: WEBENCH® Design Tools Hi everybody,
I'd like to design a rad-hard non-isolated DC-DC boost converter using the TI UC1845A-SP PWM controller.…