Part Number: UC1845A Tool/software: I am using UCI1845A as the flyback controller and the output of the IC is connected to the gate of Flyback main MOSFET through 2.5ohm. The Vcc pin is connected to 13v source hense the peak output current will be 13…
Part Number: UC1845A-SP Other Parts Discussed in Thread: UC1845A Tool/software: Hi Folks
Is the Error Amplifier biased to 5V like shown in Figure 17 or is it 2.5V shown in the functional block diagram?
Best Regards
Rolf
Part Number: UC1845A-SP Other Parts Discussed in Thread: TIDA-070002 Tool/software: Dear Support
What is the maximal peak current at the OUT pin? Specified is 200[mA] RMS but Figure 1. goes up to 500 [mA].
I saw several designs (e.g. TIDA-070002) where…
Part Number: UC1845A-EP Tool/software: Hi,
The datasheet for UC1845A-EP ( UC1845AMDREP) 8 pin-SOIC only lists thermal resistance, junction to ambient. Are there values for thermal resistance, Junction to Board and/or Junction to Case (bottom)?
Part Number: UC1845A-SP Tool/software: Dear Support
Do you provide a spreadsheed calculator for the UC1845A-SP? Or is it possible to simulate with WEBECH?
Best regards
Rolf
Part Number: UC1845A-EP Hi Experts,
Our customer would like to request information on the junction-to-case thermal resistance of UC1845AMDREP. Please provide if available.
Thank you and best regards, Gerald
Part Number: UC1845A-SP Hi,
Please provide detailed package drawing for the LCCC-20 quickly, and as a .pdf (not autocad). Part # 5962-8670408VXA (uc1845alqmlv), LDC 1915A.
The datasheet for the UC1845A-SP does NOT have the LCCC-20 (FK) package drawing…
Part Number: UC1845A-SP I have several questions below relating to setting tspec limits for the free-run oscillator frequency, the COMP offset diodes, and the Err Amp Input Voltage.
1) The oscillator: I have some DVT data from qty 3 UC1845A-SP that shows…
Part Number: UC1845A-SP Hi Experts,
Our customer would like to know if component 5962P8670411VYC uses a purely bipolar technology or, on the contrary, BiCMOS
In the second case, customer would like to know if we have any SEE reports that could share on…
Part Number: UC1845A-SP Hi,
I'm trying to set switching frequency of my flyback converter using UC1845A-SP.
I need to allo %48 duty cycle and I need fsw=300kHz. I know that Ct capacitance value effects minimum duty cycle and Rt resistance should be…