Part Number: UC2625-EP Tool/software:
Hello,
We are using UC2625MDWREP as a commutation chip which generates gate pulses for High side and low side outputs for controlling three phase BLDC Motor. With UC2625MDWREP , max 20V motor can be directly connected…
Hi Anthony,
Thanks for the response.
The RT and CT values were modified in the working board to 80.6k ohms and 10nF. The RPM decreased in a similar trend to that of non working board & will not work for our application and details as follows:-
Required…
Part Number: UC2625-EP Other Parts Discussed in Thread: UC2625 , The circuit follows Voltage control mode of UC2625. The RPM of the motor keeps increasing over a period of time from the desired RPM. lets say intented RPM is 4900 but after a duration of…
Part Number: UC2625-EP Hi
The circuit follows Voltage control mode of UC2625-EP. How to control the acceleration rate of the motor in Voltage control mode.
For our end application, the torque or acceleration of the motor has to be reduced for the same…
Hi Jan,
I apologize as I had a misunderstanding, UC2625- EP is an enhanced product, not a space product (SP) or space-enhanced product (SEP). We only provide radiation data for SEP and SP products. This product does not have available preliminary data for…
Part Number: UC2625-EP
Hi Experts,
Asking assistance and clarification on these queries:
UC2625-EP: UC2625-EP Application
In the example from the link above, they're stating that 16krpm Mech equals 62.5uS per rotation. How is this value calculated…
Part Number: UC2625-EP Reviewing a legacy product with UC2625-EP.
New to motor control and currently have no hardware to verify the following which is why I am requesting verification of the interpretation of Data Sheet and U-115 app note.
BLDC Motor…
Part Number: UC2625-EP I am utilizing the UC2625-EP device that is rated to operate down to -55C. This only happens at extremely low temperatures between -45 to -55C. I am experiencing issues with the 5V, V Ref Signal, taking a dip in voltage from 5V…
Part Number: UC2625-EPUC2625-EP
1) Would like to verify, the RC Oscillator 1-2 cycle dead time is only applied at HALL SENSORS transitions
2) Configured for four quadrant PWM , voltage control scheme, EA unity configured, EA+ control voltage with current…
Part Number: UC2625-EP Other Parts Discussed in Thread: UC2625 Using the Figure 9 (datasheet) setup for a fast high-side p-channel driver
UC2625 settings:
PWM: 200kHz
Period: 7us
Current command (To pin 1): 3.0V
Motor V: 36V
Rsense: 10mOhm
Issue: Lose…