Part Number: UC2625-EP I have plots indicating the low side gates are being driven with a double pulse. The typical PWM period is 43us.
During an event pulse separation is 13.5usec leading edge to leading edge. the first pulse is 6us wide, the second…
Part Number: UC2625-EP OV-COAST input (pin23), does it require an external pull-up when used with an open collector gate?
The Data Sheet example circuit does not employ this function, tied to GND, and the It is not explicitly stated in the Data sheet description…
Part Number: UC2625-EP Complementary FETs have the high and low side drains bonded together, preventing the insertion of the safe-braking steering diode as shown in datasheet Figure 8-C and 8-D. Would there be an issue with inserting the diode between…
Part Number: UC2625-EP Other Parts Discussed in Thread: UC3625 , Hi
This is Max.koh in korea
we will use to Motor driver ic for BG65X50CI with Motor.
So we are under review UC2625ep for them.
Could you please sent me the UC2625ep EV board Application …
Part Number: UC2625-EP Dear All;
We will use UC2625-EP brushless DC motor controller in a project. UC2625-EP has 2 types as UC2625MDWREP and V62/08624-01YE. Since V62/08624-01YE is not available now, we will use UC2625MDWREP in design. How long will UC2625MDWREP…
Part Number: UC2625-EP Other Parts Discussed in Thread: DRV8312 , Hi There;
May seem like a weird question but is there any way that the UC2625-EP could drive the DRV8312/8332? I am guessing it will require some voltage division at the PWM_X inputs?
…
Part Number: UC2625-EP Other Parts Discussed in Thread: UC2625 Hi,
I am designing a control circuit for a maxon BLDC motor, based on a UC2625 driver. The control is extremely simple: fixed speed, use of SSTART pin (or RC-BRAKE) for start/stop command and…
Part Number: UC2625-EP Hi, we're having problems with shutting the device down, when we assert the OV-COAST pin (pulling it down to GND with a MOSFET), the device draws around 100mA and gets pretty hot, which is unexpected behaviour. Is this a known problem…
Hello Furkan,
My best recommendation would be to take a look at the DRV8353M, which does have extended temp range down to -55C to support avionics applications. There is also UC2625-EP which has similar extended ratings for avionics.
DRV8343-Q1 is qualified…