Part Number: UC2825 When I used UC2825 as PWM to run half bridge converter to get 16V output. I made EA(pin1) connected to pin 3(E/A out). and Pin 2(EA NI) connected to reference pin 16 through 10K resistor. How can I determine what the fixed duty cycle…
Part Number: UC2825 Other Parts Discussed in Thread: LM25037 With the apparent release of GaN, SiC, higher frequency ferrites and so on, I currently using UC2825 for push-pull power supply which work with wide range VIN (DC) with stable VOUT (buck-boost…
Programming the frequency and dead-time is not in the "B" version of the data sheet but if you go back to the original UC2825 data sheet you can see below:
UC2825 has programmable LEB as described in section 7.1 of the data sheet:
Slope compensation…
Part Number: UC2825 Hi,
One of my customers is using the UC2825 for PWM generation. He plans to use the ramp on the CT pin for the slope compensation. In the attached figure, the comparator reference voltage is not mentioned. I saw from the Oscillator…
Aaron,
I believe your customer is asking the same questions in a parallel thread here so I am going to close this one. We do not have a Spice model for UC2825 but we have a TINA model here .
Regards,
Steve
Part Number: UC2825A Other Parts Discussed in Thread: UC2825
Hi E2E,
My customer is using the UC2825A in a buck configuration:
FETs switching at 150kHz
Output filter frequency at 300kHz
Duty cycle swing from 71% to 12% for wide input range
The issue…
Other Parts Discussed in Thread: UC2825 Hi
My customer did not find the Thermal Information of UC2825.
Could you provide the information of the RθJA, RθJC(top),RθJB.
Thanks
Part Number: UC28025 Other Parts Discussed in Thread: UC2825 What is the lot-to-lot tolerance for Maximum Duty Cycle Limit (UC28025 or UC2825), in terms of Duty cycle (%)? In other worlds, for the same RT and CT, if I change the IC on the same board,…
Other Parts Discussed in Thread: UC2825 , UCC25600 Hi Team, My customer considers to design not PWM mode(fixed frequency) but PFM mode with UC2825. He considers to input external Ramp signal to Ramp pin and not using internal OSC as the following schematic…