Hello Massimiliano,
I have two questions :
(1) Can you post the schematic for the UC2825A-Q1 section of this design ?
(2) Is the ambient or operating temperature for this test 65ºC ?
Regards
John
Part Number: UC1842A-EP Other Parts Discussed in Thread: TPS54610-EP , , UC2825A-Q1 , UC2845AQ , TPS51100 , REG1117A , REG1117 , TL1431-Q1 Hi team, Good day.
What is the ESD HBM of the following part numbers?
TPS54610-EP UC1842A-EP UC2825A-Q1 UC2845AQ…
Other Parts Discussed in Thread: LM5036 , UC2825A-Q1 , LM25037-Q1 , UCC28950-Q1 , UCC28950 Hey Team,
I'm looking for a bidirectional 48V to 12V isolated DC/DC reference design. Bidirectional is ideal, but unidirectional will work as well. Power could…
Hi Rock! Thanks so much for reaching out and for your interest in the LM5036! We are currently not offering an AEC-Q100 qualified version of the LM5036, but I strongly suggest you look into the LM25037-Q1 and the UC2825A-Q1 for some automotive qualified…
Yaita,
Here are some part numbers that appeared when I searched for your requirements. I recommend starting to look at UCC28600-Q1.
Part Number
TL2843B-Q1
UC2825A-Q1
UC2856-Q1
UC2856Q
UCC25706-Q1
UCC2813-0…
Part Number: UC2856-Q1 Other Parts Discussed in Thread: UC2825A-EP , UCC28220-Q1 Hi TI Team,
For 110 V_nom ( ±40%) input DC and 24 V (300W) output DC/DC converter WEBENCH suggests only LLC topology with controller ICs not having automotive rating…
Hi Richard,
You are correct I cant find any reference to thermal shutdown as a feature in the Q1 or EP datasheets and I have asked the design team if there is a feature in the part that performs this function.
I believe the temperatures extensions…