Part Number: UC2842AQ Other Parts Discussed in Thread: UC2842 , TL431 Hi,
I have designed 2 switch flyback converter with UC2842.
My ststem's input voltage is 200V~1000V and I designed start up circuit with depletion mosfet. I followed SLUAAL3 - figure…
Part Number: UC2842 Other Parts Discussed in Thread: UCC28C56EVM-066 Hi dear.
I designed SMPS with UC2842AQD8R. My system should start at 200V.
My start up circuit looks like this. It's now activate at 260V.
How can I make it operate at 200V?…
Part Number: UC2842AQ Hello,
I’m currently testing a prototype flyback converter that delivers 300 W output power with an input voltage range of 200 V to 1000 V and an output of 24 V .
The startup resistor is currently 293 kOhm , and the VCC capacitor…
Part Number: UC2842AQ Tool/software: We are working on a new Power supply redesign project which has got the power management IC with top marking as “ 28428 AK ISO”.
Our initial understanding is that this is a Current mode PWM Controller part UC2842AQ…
Part Number: UC2842AQ Other Parts Discussed in Thread: UC2842 Tool/software:
After the current circuit was enabled, Q2, R20, and R28 were burned out within 5 seconds. R28 will explode. I suspect that it may be due to the high duty cycle of the MOS…
Part Number: UC2842AQ Hi TI Team,
Could you please provide the temperature derating graph and Reference Short Circuit Current vsTemperature for part no UC2842AQD8R , which is not available in technical datasheet.
Part Number: UC2842AQ Hi,
We are using UC2842AQ in Two switch Forward converter Topology - Vin = 32, Vout = 12, Transformer ratio 1:2, Load 14.13A, Freq 150KHz.
We are operating the Regulator at Current Mode. The regulator would always be in CCM…
Other Parts Discussed in Thread: UC2842AQ
Hi all, Would you mind if we ask UC2842AQ? In case of TA -40℃ to 125℃, if you have following datas, could you send me? We will use these as reference data. -Temperature characteristic of Maximum Input Signal…
Part Number: UC2842A Hi,
I have read datasheet of UC2842A and application circuit ( calculation ).
Questions :
1. Snubber Circuit ( RCD snubber selection ) Calculation not specified ? Please give the calculation details.
2. Is there any Simulation…