Part Number: UC2843A-Q1 Other Parts Discussed in Thread: UC2843 Hi, anybody have the any reference Tina Model / ref schematic for UC2843 which can take DC input of 75-150V and convert it to 14V, 10A.
Part Number: UC2843A-Q1 Am planning to use this Driver IC for our design,
I need some clarification on this. When I'm doing WEBENCH with the UC2843A-Q1, there is an ISENSE pin in that circuit. I understand that it is used for sensing the current from…
Part Number: UC2843A Hi,
I want use UC2843A in my flyback power design, and I used WEBENCH to generate a reference.
Now I have a question about the c urrent ripple rate , why the current ripple rate recommended here is not 0.3~0.5? As many switching power supply…
Part Number: UC2843A-Q1 Other Parts Discussed in Thread: UCC2897A Hi ,
Can UC 2843 used for below application ?Is it right choice if not please suggest suitable alternate .
Fly back isolated converter
Input DC =25V ~ 100V
Output DC = 14V /10A .
Ambient…
Part Number: UC2843A Hi Team,
During test, we find there is negative spike on OUT pin. Please kindly help check if it's OK.
There is -0.5V/80ns spike.
BRs
Given
Part Number: UC2843A Other Parts Discussed in Thread: UC3843 i am boulding a current limiting brushed DC motor power supply
DC to DC. buck only
my input voltage ranges from 8 to 35V nominal 12V the
motors maximum voltage is the input voltage motor current…
Part Number: UC2843A-Q1 Hi team,
The operating temperature range of the UC2843A-Q1 is -40 to 125°C on the product page, but 6.3 of the data sheet lists it as -40 to 85°C. Which is correct?
Thanks Ryu
Part Number: UC2843A Other Parts Discussed in Thread: UC3845 , UC3843 , UC3842 , UC3844 , TL494
Dear TI experts,
The following are the circuits on our new product, please help to review whether there is any problem with the design, thanks!