Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Hi Seshaiah,
Thank you for the query on UC2854.
Please refer page-3 for the following link for the difference:
https://www.ti.com/lit/ds/symlink/uc3854.pdf?
DDW refers to the package also mentioned in page3.
Regards,
Harish
Dear Harish,
Thank you for your response.
The UC2854 was added as one of the candidates because it can be used in the range of 0-85C. (Not enough for 100C...)
Can UC2854, UCC28180 and UCC28019 be used with 4000W output?
By the way, in the current concept…
We are designing a 220VAC input 10KW power supply. Front end is a 2854 based PFC stage.
I put a 75 ohm to it and raises input from 0VAC, the PFC starts to work from 20VAC, boosts to 200VDC or so, at 30VAC it regulates at 400VDC, PF 0.982. However when…
Part Number: UC2854A Other Parts Discussed in Thread: UC2854 In the original version of the IC (UC2854) Multiplier current was limited to 3.75V/RSET.
In this version of the IC, the datasheet indicates that maximum multiplier current is limited to 2xIAC…
Hello,
This device should have similar ESD ratings compared to the uc2854.
According to the UC2854 data sheet section 7.2, page:
HBM = +/- 2500V
CDM = +/- 1500V
Regards,
Part Number: UCC2818 Other Parts Discussed in Thread: , , UC2854 , UC2854B , UC2854A , UC3854A , Hi team,
Customer has a question regarding the UCC2818 (and its equivalents like UCC2818-EP and UCC2818A-Q1): What is the voltage at the IAC input?
This pin needs…
Other Parts Discussed in Thread: UCC28070 , UCC29910A , UCC28180 , UC2854 Hi all,
I have to design 600W buck PFC circuit.
Please suggest us IC/ Design/ circuit to meet below specifications
1. Vin: 90- 265 Vac, 1 phase , 50 Hz
2. Vout: Any value between 60…
Part Number: UCC3817 Other Parts Discussed in Thread: UC2854 , , UCC28180 My question or observation concerns the PFC part differences between the ucc3817 vs. UC2854 units
The internal multiplier output (Imo) is hard-connected either to the inverting or non…