Other Parts Discussed in Thread: UC2854B-EP C2854B-EP ; SGLS318A –NOVEMBER 2005–REVISED NOVEMBER 2015 That is the datasheet i'm looking at UC2854B-EP Advanced High-Power Factor Preregulator UC2854B-EP SOIC (16) 10.30 mm × 7.50 mm …
Other Parts Discussed in Thread: UC2854B Hi Ti Team,
Client specifically requires above Part number.
So please kindly share the LTSpice model for the above Partnumber,
Part Number: UC2854B Other Parts Discussed in Thread: UC2854 Can we have a clear explanation on the difference between UC2854DW, UC2854ADW, UC2854BDW?
We are in need of UC2854BDW parts around 2000 qty, for regular production of welding equipment.
We need…
Part Number: UC2854B Other Parts Discussed in Thread: UCC28180 , UCC28056 , UCC28070A , UCC28063A , UCC28064A , UCC28065 Hi experts
I see that no behavioral models are available for the UC2854B.
Can someone recommend some similar newer devices with equivalent…
Part Number: UC2854B Other Parts Discussed in Thread: UCC3818 , UCC28070 CURRENT ERROR AMPLIFIER
This error amplifier configuration conventionally has a resistor from the inverting input to common, and a resistor from the multiplier output to a negative…
Part Number: UC2854B-EP Other Parts Discussed in Thread: UC2854B , , UC2845 Hi,
I am currently designing a PFC with a boost topology.
In my design, it is preferable to use an external op amp to do the voltage loop function,
The output of this external op…
Part Number: UC2854B-EP Other Parts Discussed in Thread: UCC2818-EP , Hi,
The UC2854B-EP has the same functional bloc as UCC2818-EP, better current amplier bandwidth, low gain dispersion of multiplier but requiere more supply current and it is more expensive…
Part Number: UC2854B-EP Other Parts Discussed in Thread: UC2854B , Regarding a 400Hz 115Vac input PFC module for military avionics application:
In doing higher temperature testing (baseplate > 70 deg C), the THD begins to increase from ~3% to ~10% (seems…
Part Number: UC2854B Hi, I want to design PFC using UC2854B under the following conditions. Input : AC85V-265V, DC125V(-10%, +15%) Output : DC390V 200W Efficiency : 90% Switching frequency : 65kHz
In this case, can UC2854B be used with both of AC and DC…