Part Number: UC2854B-EP Other Parts Discussed in Thread: UCC2800-EP , UCC28C55-Q1 Hello,
We are currently using UC2854BMDWREP in our design. At the time of component selection, the part had a YTEOL (Years to End of Life) of approximately 15 years according…
Part Number: UC2854B-EP Other Parts Discussed in Thread: UC2854 , UC1854 Hi
I am using UC2854 for 115V, 360Hz to 30V convertion for 15W power supply, For room temperature gate pulse starting at 2nd negative cycle itself, but while testing at 110deg…
Part Number: UC2854B-EP Other Parts Discussed in Thread: UC2854B , Tool/software: Dear TI Team,
In the UC2854B-EP datasheet, the operating voltage values appear to be contradictory. For your reference, I have attached an image showing the issue…
Part Number: UC2854B-EP Other Parts Discussed in Thread: UC2854 , UC2854B , Tool/software:
Hi Team,
I need to know the voltage on the Vref pin of the PFC controller when I apply 0V to the Enable signal and 15V to the VCC pin of the controller. Will…
Part Number: UC2854B-EP Tool/software: Dear TI Team,
I am designing a PFC system for an aircraft application with an input operating range of 90Vrms to 134Vrms and a frequency range of 360Hz to 800Hz .
The peak load for the design is 300W , while…
Other Parts Discussed in Thread: UC2854B-EP C2854B-EP ; SGLS318A –NOVEMBER 2005–REVISED NOVEMBER 2015 That is the datasheet i'm looking at UC2854B-EP Advanced High-Power Factor Preregulator UC2854B-EP SOIC (16) 10.30 mm × 7.50 mm RθJC Junction-to-case…
Part Number: UC2854B-EP Other Parts Discussed in Thread: UCC2818-EP , Hi,
The UC2854B-EP has the same functional bloc as UCC2818-EP, better current amplier bandwidth, low gain dispersion of multiplier but requiere more supply current and it is more…
Part Number: UC2854B-EP Other Parts Discussed in Thread: UC2854B , , UC2845 Hi,
I am currently designing a PFC with a boost topology.
In my design, it is preferable to use an external op amp to do the voltage loop function,
The output of this external…
Part Number: UC2854B-EP Other Parts Discussed in Thread: UC2854B , Regarding a 400Hz 115Vac input PFC module for military avionics application:
In doing higher temperature testing (baseplate > 70 deg C), the THD begins to increase from ~3% to ~10% …
Part Number: UC2854B-EP Hi TI-team
My customer is using UC2854B-EP.
Normally, I think ENA operates at 2.35V or more.
However, there is a sample that operates with ENA around 1.9V.
VCC at this time is about 10.5V.
Vref also outputs 7.5V.
…