Part Number: UC3525A Hello all,
I'm just curious about the series resistor in the 10 input pin. Why in some parts of the datasheet of the UC3525 is shower a 3K, and in others you can see a 5K resistor? Could be a mistake?
Thanks!
Part Number: UC3525A Hello all!
Last week I asked to your support team about Figure 10 of the UC3525 datasheet. I was worried about how this circuit could work and I asked for a example. Without answers.
See, in a first sight this circuit converts…
Part Number: UC3525A Hi TI team
I'd like to know output A & B of UC3525A.
Are they reverse each other, or phase difference angle??
I want to combine the two output to achieve a 99% duty cycle.
Could it be possible?
Thanks
Part Number: UC3525A Hi Experts,
My customer is asking about abs max of SHUTDOWN pin.
I am guessing it is max 5.5V (logic input) but please let me confirm because SHUTDOWN pin is the base of internal NPN transistor which requires the bias current…
Hi Can! Thanks for reaching out! The error amplifier on the UC3525A is not an OTA. You can use type 3 compensation with a full bridge converter using the UC3525. Here are a couple documents to help you get started: Compensation Made Easy and Demystifying…
Part Number: UC3525A Hi team,
Could you kindly advise the below inquires form customer ?
1. Why the charge time at CT 0.1uF in Fig 1 is longer than at CT 0.02uF ? It seems the number of CT get be smaller and smaller and charge time get be longer as…
Eamonn - How are you !!! - long time no see and welcome to the TI e2e forum !
Anyhow - to answer your question
The duty cycle isn't a strong function of input voltage so if the design was working ok over the 3 to 60V range the duty cycle shouldn't…
Part Number: UC3525A Other Parts Discussed in Thread: MC34063A , , LM5119 , PMP10979 , LM25119 Hello, I need to design a buck converter that will limit the voltage in an automotive-type dc system. The input may be from 11 to 15 volts; the output should…