Part Number: UC3708
Hello.
I hope you are doing well. I am designing a prototype for my master's thesis and due to some technical issues I can only use through hole components. I have found UC3708, but unfortunately the technical datasheet does not…
Part Number: UC3708 Other Parts Discussed in Thread: UCC27524 Hi,
I suspect typo of the datasheet.
Could you check if following unit is correct?
Best Regards,
Kuramochi
Is it possible to apply a voltage bigger than 5.6V to the ENABLE input?
The absolute maximum rating indicated in the datasheet is 5.6V, but the equivalent electrical input circuit shows two decoupling diodes that should allow bigger voltages to be applied…
Part Number: UC2950 Other Parts Discussed in Thread: UCC27624 , UC3708 , UC3709 Hi,
Do you have a half-bridge gate driver that meets the following criteria? I searched TI HP, but I could only find a product that drives two Nch Switches.
[Conditions…
Hello,
Thanks for your interest in our driver.
UCC27524A is an industry standard dual channel driver targeting wide broad applications where thermal shutdown is not necessarily required from the driver.
UCx708 family, part of our dual channel might…
Hi Takahiro-san,
Thanks for your interest in our device, my name is Mamadou Diallo, I am the AE supporting low-side drivers.
This is an older device, therefore the data may not be readily available. However depending on specific features of interest…
Hello Kai,
I am an application engineer at TI supporting low side drivers and will address your question. TI does offer a dual driver with up to 35V operation which is the UC3708. This is an older bipolar device however, so you may want to consider…