Part Number: UC3825A Other Parts Discussed in Thread: UC3825 ,
This is an applied circuit diagram, with pins 11 and 14 connected to the gate driver and full bridge MOS to obtain the final voltage output in the upper left corner. And this voltage output…
Part Number: UC3825 Other Parts Discussed in Thread: UCC28220 Hi TI team,
I have a question about the synchronized operation of the UC3825 IC.
In synchronized operation, PWM outputs of master and slave also can be synchronized?
Part Number: UC3825 Other Parts Discussed in Thread: UC1825 , I have experienced some problems with the UC3825 when operating at low duty cycles. The device controlles a symmetrical half-bridge converter, oscillator is set to 380kHz, LEB is set to minimum…
Part Number: UC3825
Hi,
I am using it Full bridge converter configuration. Input dc is 250V to 380V. Output is variable from 0 to 200V. I am observing Only one pulse release in one of the two PWM output's for lower load or low voltage conditions(around…
Part Number: UC3825 Other Parts Discussed in Thread: UCC28950 Hi
Can I find the minimum duty of the UC3825 PWM IC? If you have a product with a lower minimum duty, I would highly recommend it.
In addition ucc28950 will be applied to the next model. I want…
Part Number: UC3825A Other Parts Discussed in Thread: LM5045 , UCC28950 Hi,
I am using UC3825DW IC for PWM generation at 350kHz for resonant full bridge inverter . This is operated at 17volts ac. Rc=1.39kOhms and Ct=1.22nF. This IC getting heating up very…
Part Number: UC3825 Hi TI e2e Members
I am using UC3825 for single switch forward converter application. I am using IC in current control mode. I am having some doubts regarding this IC.
link to datasheet : www.ti.com/.../uc3825.pdf
From the page number…
Part Number: UC3825 I use UC3825AN and UC3823AN for experiment. In my researches, I use peak current mode control converters. First I have doubt with error amplifier. Saturation of this is 5V. But I want to know that saturation voltage can be increased…