Part Number: UC3842 Tool/software:
Objective: Implementing External Over Voltage Protection (OVP) for UC3842
According to the UC3842 datasheet, the shutdown technique section describes how to implement external over voltage protection using an external…
Part Number: UC3842 Tool/software: Dear TI community
We want to design a power converter of 600W. My input and output specification are 230VAC and 60VDC at 10A. please suggest the topology and control ic.
Is there any possible for using the flyback…
Part Number: UC3842 Tool/software:
I am designing a topology with a high input DC voltage of 800V.
In the case of a ceramic capacitor used to eliminate common mode noise between the ground of the primary side and the secondary…
Part Number: UC3842 Tool/software: when designing a flyback converter using the UC3842 IC with an input range of 200V to 1000V and a 24V output
would it be appropriate to use a 280kohm start-up resistor?
according to the datasheet, the maximum start…
Part Number: UC3842 Dear All,
I am making a flyback converter using UC3842 (Output 12V, 12W, Input 100V-220V). The desired voltage is 12V however, the initial output when the feedback resistor was 9.5k was 21 V . When the Feedback resistor Rf was changed…
Part Number: UC3842 Other Parts Discussed in Thread: UCC28C56EVM-066 , UCC28C56H Tool/software: Hi,
I’m working on designing an SMPS using the UC3842 IC. My topology is a conventional flyback converter without any special techniques.
However, my input…
Part Number: UC3842 Tool/software: Hi Ti Team,
I am using UC3842 IC for 250W Flyback converter for charging application
when i turned ON giving input from Variac(0 to 230V )AC converter works fine,but when i give direct 230V AC converter Fails,shunt…
Part Number: UC3842 Other Parts Discussed in Thread: LM5148 , LM25190 , LM25149 , TL494 , Tool/software:
Hi,
We are currently supporting a customer who is designing a non-isolated buck converter with the following conditions:
・Input voltage: 18V…
Part Number: UC3842 Hi
Ii want to simulate the Forward Converter using UC3842 in Ti power Stage Designer tool. Whether the Ti Power Stage Designer tool is free..
Thanks
Ganesamurthy