Part Number: UC3907 Other Parts Discussed in Thread: UCC29002 Hi guys,
Does this Load Share Controller also work with constant current power supplies? If not is there an alternative that you can recommend?
If there are no Load Share Controllers for…
Part Number: UC3902 Other Parts Discussed in Thread: UC3843 , UC3907 , , UCC39002 Hello I used UC3843 to make a positive power supply.
I want to increase the current sharing function.
I found that both UC3902 and UC3907 can achieve current sharing…
Part Number: UCC39002 Other Parts Discussed in Thread: UC3907 Dear TI friends:
I have a qurestion,so canyou help solve it? for UCC39002 or UC3907, I want to connect multiple power supplies with Sense function into shunt output, I wonder if it is ok…
Other Parts Discussed in Thread: UC3907 I am using this load share controller and am looking to provide a status signal when the overall load exceeds a certain amount.
Hi all,
Is there any UC3907 Pspice model , I looked all over TI website and didn't find any , can I at least get the different parameters of the IC so i can build it on my if there's no model available.
looking forward to hearing from you.
Thank…
Other Parts Discussed in Thread: UC3907 We have two 24V duplicate DC supplies and are using the UC3907 on each to share the load between these two supplies. What we are finding is that the load is not equally shared. At some point one supply is allowed…
How calculate the values from voltage loop compensation between pin 12 and pin 11
what the voltage max generate by pin 9
can i use this controller with UC 3525 and how?
Thank you very much
Part Number: UCC29002 Other Parts Discussed in Thread: UC3907 Hi Team,
Posting on behalf of our customer.
We’re designing a current-sharing scheme, and while reading the UC3907 documentation I noticed it uses a differential signal to minimize line…
Part Number: UC2907 Other Parts Discussed in Thread: UC3907 Hi,
I am test engineer looking to test a UC2907 TI Datasheet SLUS165C. Can a test circuit be provided for a typical application which includes this device?
Thanks,
Joey
Part Number: UCC29002 Other Parts Discussed in Thread: UC3907 , UCC39002 , TL431 Hi,
How can the UCC29002 get away without the 50mV voltage offset that is needed in uc3907 to stop the master trying to adjust its own reference?