Part Number: UCC12041-Q1 Other Parts Discussed in Thread: UCC12051-Q1 , Tool/software: Hello expert,
Here are a few customer questions about EMI test, pls help support it:
1. The EMI test report is for UCC12051-Q1 not UCC12041-Q1 in the TI website, is UCC12051…
Part Number: UCC12041-Q1 Hi expert,
It was found that there was no output capacitor, the UCC12041-Q1 chip was very hot. Could you help analyze what the reason for this phenomenon? thanks.
BR,
Hangjie
Part Number: UCC12041-Q1 Hi team,
I have a question. As the datasheet mentioned, the operating current in no-load seems to be higher than I expected. What is the reason of this high current consumption.
Best Regards,
Part Number: UCC12041-Q1 Hello Sir:
We saw two package drawing on datasheet.
One package shows IPC-7351 NOMINAL 7.3 mm CLEARANCE/CREEPAGE and the other one shows HV / ISOLATION OPTION 8.1 mm CLEARANCE/CREEPAGE.
Please let us know which package drawing…
Part Number: UCC12041-Q1 Other Parts Discussed in Thread: UCC21750-Q1 Hello,
I understood that, when AIN is > 0.6V, a PWM signal appears on the APWM output (The Duty cycle is the image of the voltage applied to the AIN input)
Could you please let me…
Part Number: UCC12041-Q1 Hi Team, The datasheet says to put a 100 kΩ pull-up resistor on the SYNK_OK pin, but I do not need output confirmation on the SYNK_OK pin. In such a case, is it safe without a pull-up resistor? Regards, Hamashima
Part Number: UCC12041-Q1 Other Parts Discussed in Thread: UCC12051-Q1 , Hi This is Pranay. I need an isolated DC-DC converter IC or DC supply with isolation. We have finalized UCC12041-Q1 and UCC12051-Q1. These two ICs will provide isolated DC-DC power supply…
Part Number: UCC12041-Q1 Other Parts Discussed in Thread: UCC12040 , Hi team,
What is the difference between UCC12041-Q1 and UCC12040? The electrical characteristics are almost the same, but why are the model numbers ending differently?
Best Regards,
Part Number: UCC12040 Other Parts Discussed in Thread: UCC12050 , UCC12051-Q1 , UCC12041-Q1 Hi,
Am I correct in understanding that the difference between UCC12050 and UCC12040 is the insulation barrier (5kVRMS, 3kVrms), and that other electrical characteristics…
Suma,
I assume you are trying to bias a high-side referenced gate driver that will be used to drive a SiC? The UCC12041-Q1 is a 5 V-to-5 V module and will not meet your requirement of 15 V output unless you stack three outputs to get 3x 5 V=15 V. This…