Part Number: UCC12050 Hi expert,
I found there's also CMTI definition here for such kind of isolated parts, except isolator and isolated gate driver.
As explained in this app note: Common Mode Transient Immunity (CMTI) for UCC2122x Isolated Gate…
Part Number: UCC12050 Other Parts Discussed in Thread: UCC12040 , Hi support team,
Please let me know the meaning of "Revision History" of SNVSB38D.
Page-17: Added Section number included.
Does that mean the position in section 7.4 has moved? …
Part Number: UCC12050 Hello
The EVM datasheet [SLUUBD5C – SEPTEMBER 2019 – REVISED JUNE 2021] recommends:
" 4.1 Pin Functions ... EN Active-high enable input. Connect EN to GNDP to disable the device. Connect EN to VINP to enable the device…
Part Number: UCC12050 Can confirm that the UCC12050 has a power dissipation of 385 mW with only 50 mA of current load (Iiso) ?
Below my technical analisys.
The following table is taken from datasheet of UCC12050, Power Ratings
Defining Pboard the board…
Part Number: UCC12050 Is it possible to use 2 UCC12050 in series to create a 10.8Vdc 90mA isolated supply ? i.e. GNDS of 2nd UCC12050 will sit on Viso of first one.
Love the UCC12050 for functionnal safety products. It would be nice to have variations…
Part Number: UCC12050 Hi Team, need your inputs on this concern.
Need to parallel 3 of these devices for the power level required. Initially attempted using or'ing diodes on the output of each DC-DC, but have found we have devices failing in the testing…
Part Number: UCC12050 Other Parts Discussed in Thread: UCC12040 , ,
Unfortunately, we have noticed high EMI with our new PCB. The UCC12050 isolates +5V from USB to other circuitry, and part of the EMI passes to the USB cable. Additional filtering here might…
Part Number: UCC12050 Please let us know pin treatment of SYNC_OK pin at standalone operation.
SYNC ---> connect to GNDP
SYNC_OK ----> Pull up to VINP ?
Regards,
Part Number: UCC12050 Other Parts Discussed in Thread: SN6505B , SN6505A , Hi
My customer wants to confirm whether the output can be 0.5A Or suggest a suitable product Input 5V to Output 5 V Current 0.5A
Thank you