Part Number: UCC12050 Is it possible to use 2 UCC12050 in series to create a 10.8Vdc 90mA isolated supply ? i.e. GNDS of 2nd UCC12050 will sit on Viso of first one.
Love the UCC12050 for functionnal safety products. It would be nice to have variations…
Part Number: UCC12050 Hi Team, need your inputs on this concern.
Need to parallel 3 of these devices for the power level required. Initially attempted using or'ing diodes on the output of each DC-DC, but have found we have devices failing in the testing…
Part Number: UCC12050 Other Parts Discussed in Thread: UCC12040 , ,
Unfortunately, we have noticed high EMI with our new PCB. The UCC12050 isolates +5V from USB to other circuitry, and part of the EMI passes to the USB cable. Additional filtering here might…
Part Number: UCC12050 Please let us know pin treatment of SYNC_OK pin at standalone operation.
SYNC ---> connect to GNDP
SYNC_OK ----> Pull up to VINP ?
Regards,
Part Number: UCC12050 Hi expert,
My customer is wondering if we have some test data that could show relationship between life and operation temperature of UCC12050? Or if we have some data that show failure rate of UCC12050 working at very high temperature…
Part Number: UCC12050 Other Parts Discussed in Thread: SN6505B , SN6505A , Hi
My customer wants to confirm whether the output can be 0.5A Or suggest a suitable product Input 5V to Output 5 V Current 0.5A
Thank you
Part Number: UCC12050 Other Parts Discussed in Thread: UCC12040 Hi Team, Is this design implementation of our customer possible for UCC12050? They want to connect the outputs of two UCC12050 converters in series to achieve 5V, GND and -5V
Please let me know…
Part Number: UCC12050 Dear Specialists,
My customer'd like to know where to connect SYNC_OK pin when unused.
SYNC_OK pin is Open Drain, generally it should be open, is it correct.
I appreciate your great help in advance.
Best regards,
Shinichi