Part Number: UCC12041-Q1 Other Parts Discussed in Thread: UCC12051-Q1 , Hi This is Pranay. I need an isolated DC-DC converter IC or DC supply with isolation. We have finalized UCC12041-Q1 and UCC12051-Q1. These two ICs will provide isolated DC-DC power supply…
AnBer,
The device is 10 kVPK surge rated and qualified according to IEC latest standard IEC 60747-17 (previous was DIN VDE V 0884-11). If you look at the test conditions for the VDE it states 1.6 x VIOSM. VIOSM is 6250 VPK and 1.6*6250 VPK=10 kVPK. When…
Hi Feeney,
Based on the diagram you've provided, I don't think I would recommend UCC2803 as a stand alone isolated current sensing solution. Isolated Current Sensing Solution or Design considerations for isolated current sensing are two good TI references…
Part Number: UCC12040 Other Parts Discussed in Thread: DCPA10505 , , UCC12051-Q1 , UCC12041-Q1 , UCC12050 Hi support team,
I want to input 5V and output 5V isolated voltage. The output current is 7mA and I am using DCPA10505, but the output voltage becomes…
Other Parts Discussed in Thread: UCC12040 , UCC12051-Q1 , UCC12041-Q1 , UCC12050 Hi,
my customer is looking for p2p alternative to ADUM6028-5BRIZ
The BOM tool does not find anything.
Do we have anything?.
BR Josef
Part Number: UCC12040 Other Parts Discussed in Thread: UCC12050 , UCC12051-Q1 , UCC12041-Q1 Hello,
Can you please elaborate on the applications of the UCC12040, and in particular the "Isolated voltage and current sensing" mentioned in the datasheet?…
Part Number: UCC12050 Other Parts Discussed in Thread: UCC12040 , UCC12051-Q1 , Hello,
We would like to check whether the SYNC input pin can be driven with an external 3.3V clock signal, which seems feasible based on the datasheet.
Could you please confirm…