Part Number: UCC14141-Q1 Other Parts Discussed in Thread: UCC14141EVM-068 Tool/software: Dear team,
The customer would like to use UCC14141-Q1 for bias supply.
Customer specification is below.
- VDD : 2V, VEE : -18V
But using calculator, As you can see…
Part Number: UCC14141-Q1 On page 9 of the datasheet from June 2023 in chapter 7.6 the safety-related certificates are missing. When will this be added, especially according to DIN EN IEC 60747-17 (VDE 0884-17)?
Part Number: UCC14141-Q1 Hi,
Customer is using UCC14141 for PTC heater project.
There is an issue with EMC testing.
Please give me some advice on how to improve EMC for UCC14141.
Schematic :
CE(Conducted Emission)
Using UCC14141-Q1 : 45 to 100 MHz band…
Part Number: UCC14141-Q1 Hi,
Can you tell me how to build the orderable device reference of the UCC14141 to have the version with Vin = 8V to 18V and not the 19.8V to 13.2V version? I couldn't find how to differentiate the 2 versions in the datasheet…
Part Number: UCC14141-Q1 Other Parts Discussed in Thread: TPSI3050-Q1
Hi Team,
Good day !!
Please help me with Power consuption of IC when we configure UCC14141-Q1 in below configurations:
1. UCC14141-Q1 with Two-wire system: if it is driver B-B MOSFETs…
Part Number: UCC14141-Q1 Hi,
The customer encountered an issue during the UCC14141 test.
It is confirmed that a fault occurs due to overcurrent at the output end and Retry is not possible with the output turned off.
The MCU is located in the high voltage…
Part Number: UCC14141-Q1 Hi,
I am using the UCC14141-Q1 chip as a gate drive power supply for my application. I am using the design calculator tool to estimate the component values.
I would like to understand how to estimate the below values of the gate…
Part Number: UCC14141-Q1 Hi TI Team,
I have used 4* UCC14141.in my prototype board to supply a H bridge. and I configure it as VDD-VEE 23.5V, COM-VEE 3.5V.
when I power on the board, all 4 unit works fine. and I can hear some ring noise in all these 4…
Part Number: UCC14141-Q1 Our customer would like to to use UCC14141-Q1 with single output.
Please let us know how should they set the resistance value of RLIM?
regards,
Kura
Part Number: UCC14141-Q1 Hi,
The customer is reviewing UCC14141 for the high voltage PTC heater project.
UCC14141 operating voltage range : 8 ~18 V.
Falling voltage of UVLO is typ 7.4V.
Rising voltage of OVLO is typ 22V.
The PTC heater must be a warranty…