Part Number: UCC14240-Q1 HI,
Would wish to know if the UCC14240 can be used in a SSR type application where the SiC FET is turned on with 20V and turned off with -5V .Here the ON signal will be a continous high signal unlike the PWM .If possible what…
Part Number: UCC14240-Q1 In the Rev. C datasheet Table 8-1 it says "For extreme input ripple voltage cases, connect a 4.75-ohm filter resistor to power input, PIN7, and connect a 10-μF ceramic capacitor from analog VIN PIN 6, to power analog GNDP…
Part Number: UCC14240-Q1 Other Parts Discussed in Thread: UCC14131-Q1 , UCC25800-Q1 Hi
Could you help suggest suitable products ,
Automotive displays must pass VSCC 56-3 The car power supply provides DC 24V, and the motherboard provides DC 12V.
So DC to…
Part Number: UCC14240-Q1 Hi,
I was aware there was some testing being done on whether having UCC14240-Q1 and iso gate driver on exactly opposite sides (rather than side-by-side as in EVMs) will have any negative consequences (possibly impact from UCC14240…
Part Number: UCC14240-Q1 Other Parts Discussed in Thread: UCC25800 , UCC14140-Q1 , UCC25800-Q1 Hi, The UCC14240-Q1 device uses a two switch "balancer-like" topology to regulate the COM-VEE voltage (Figure 7-2 in the UCC14240-Q1 datasheet). Does…
Part Number: UCC14240-Q1 Other Parts Discussed in Thread: UCC14240EVM-052 Hi, I try to understand the Application Note "UCC14240-Q1 Simplifies HEV, EV, Bias Supply Design for Isolated Gate Drivers" (SLUAAH0). In chapter 7 on page 13, Equation…
Part Number: UCC14240-Q1 Hi team,
(1) How do we deal with unused /PG pin? Could we tied it to GNDP? Or is pull up resitor needed for its correct operaion evne though we do not monitor /PG voltage?
(2) Does "ENA-pin" has intenral pull-down resitor?…
Part Number: UCC14240-Q1 Dears:
when customer use UCC14240-Q1 to build a board , they found below issues:
1-they found when Vin rise slope is very sharp such as 8mS, UCC14240-Q1 can not start and there is no output voltage.
2-when Vin is around 22V, even…