Part Number: UCC14241-Q1 Tool/software: Dear TI expert,
We're designing SiC gate driver power supply with UCC14241. Common mode choke is typically required in the input of power supply.
- What is the recommendation for CMC with UCC14241
- Addition…
Part Number: UCC14241-Q1 Tool/software: Hello Team,
Can you share with us the package information about Tape and Reel Box dimensions (Length, Width, Height)?
This is not available in the datasheet.
Regards,
Renan
Part Number: UCC14241-Q1 Hi team,
I see that the UCC14241QDWNRQ1 was tested to JESD22-A104 temperature cycling profiles. What is the profile for those tests? Temperature and soak time?
Any details on the profile are appreciated.
Thanks,
Jacob
Part Number: UCC14241-Q1 Hi sir
I want to design the power module in ATE system
as you know ,ATE is a instrument with Accurate measurement
so we need to check all the parts less noise in the circuit
Question:
1.check high frequency radiation & noise…
Part Number: UCC33420 Other Parts Discussed in Thread: UCC14241-Q1 Tool/software: Hello,
I entered a random product code just to get a product recommendation.
We are looking for an isolated supply for a 3-phase motor driver system that steps down from…
Part Number: UCC33020-Q1 Other Parts Discussed in Thread: UCC33420-Q1 , UCC14241-Q1 Tool/software: In order to have a higher power output, is it OK to connect multiple UCC33020-Q1's output VCC in parallel directly? Or, do they have to go through a diode…
Federico,
A few recommendations to get you started:
Suggest to use UCC14241-Q1 or UCC15240/1-Q1. All are p-2-p compatible with UCC14240-Q1. Versions that end with "1" are 5kV isolation, versions that end with "0" are 3kV isolation and 15240/1 vs 14241…
Part Number: UCC14240-Q1 Other Parts Discussed in Thread: UCC14241-Q1 , Tool/software: Hi, I'm designing a power supply for my gate driver.
The specifications for the gate driver are:
VCC: 15 V
VEE: 8 V
However, I am experiencing excessive ripple…
Part Number: LM25183 Other Parts Discussed in Thread: UCC14241-Q1 , UCC15241-Q1 Tool/software: HI team,
Could you help check if we have alternative of MID1W2424A?
24-24V, 1.5W, Isolated DC/DC Converter With 5kV RMS Reinforced Isolation, with an integrated…
Here are some recommended debug steps:
For new designs, change UCC14240-Q1 to UCC14241-Q1. UCC14241-Q1 has some startup and noise immunity improvements that were not captured in UCC14240.
Please follow the PCB design guidelines detailed in section 12…