Part Number: UCC20520 Tool/software: HI TI expert,
Customers use the UCC20520 device, as the mos current size changes, the delay varies between 800-900ns, the larger the current, the longer the delay.
Oscilloscope waveform primary waveform - green…
Part Number: UCC20520 Tool/software: We are using the UCC20520 with a 100K dead time resistor and 2400pF capacitor in parallel. The chip still does not give us any dead time. We have tried it with a 205K resistor also with no change. Any ideas on what…
Part Number: UCC20520 Hi,
I am using UCC20520 isolated driver for 15 phase inverter.
So I am wondering if I can design each driver (15 driver pcb) with its own supply and its input filter or use a power managment board able to provide filtered 12V…
Part Number: UCC20520 Hi,
I'm working on an inverter and i'm using the UCC20520 as a gate driver as you can see in the schematic below.
U2 is a DC/DC that supplies the secondary of the driver.
U5 and U7 are two differential drivers that we added…
Part Number: UCC20520 Other Parts Discussed in Thread: UCC21530 Hi team,
How does TI classify if the specific isolated gate driver supports certain type of power switch exactly?
Do we have any quantatative criteria to classify gate drivers such as…
Part Number: UCC20520 Hi,
I'm working on a single phase inverter using SiC Power Module and i'm using the UCC20520 as a driver. While doing a double pulse test and i found that the PWM signal is very disturbed as you can see in the picture below,
…
Part Number: UCC20520 Hi team,
My customer has a question on the UCC20520..
Is there an internal pull down resistance from gate to source? From looking at the datasheet, it appears not. But if not, what kind of leakage currents can they expect between…
Part Number: UCC20520 Other Parts Discussed in Thread: UCC21520 Hi Team,
Just double check, is pin2 internally not connected to anything?
Customer met UCC21520 shortage, and don't want to spin another ver. change so checking if it's ok applying PWM…
Part Number: UCC20520 We have an old module with SI8231 for AC voltage stepup (Similar to Class D amplifier)
I have checked and found both the ICs pin compatible. Advantage of using UCC20520 would be having simulation model available to avoid a spin…