Part Number: UCC21220A There is not material content for UCC21220ADR in ti.com. Customer need that for the AVL code setup. Could you pleas help check for it? Thank you.
Part Number: UCC21220A Hi,
We are using a UCC21220A Gate driver to run 10 IRF135B203 MOSFETs in parallel for our 450ARMS, 78V motor controller. While testing the device we have observed a distorted Vds waveform while running at higher currents. At 325A…
Part Number: UCC21220A Hi team,
Here is an item want to confirm with you.
there is a formula as following which is used for caluculating the actual source current:
how to understand the minimum function here? And the 4A peak source current spec understanding…
Part Number: UCC21220A Other Parts Discussed in Thread: LMG1205 , LMG1020 , LMG1210 , ISO6721 Hi,
I'm looking at a 3-phase 48V, 22A peak H-bridge and want to use an EPC2022 as the transistor. I know I can use a LMG1205 etc as the driver for a non-isolated…
Part Number: UCC21220 Hi Team,
My customer needs to meet IEC 60950-1 and IEC 62368-1 on their end equipment, could UCC21220 & UCC21220A comply with these 2 certifications?
BTW, may I confirm the progress on DIN EN 61010-1 and GB4943.1-2011? The status…
Part Number: UCC21220A Other Parts Discussed in Thread: UCC21220 , UCC21220EVM-009
Power supply designers are often challenged to make their systems solutions more efficient, more reliable, and smaller in size, while still maintaining competitive pricing…
Part Number: UCC5304 Other Parts Discussed in Thread: UCC21220A , Is there a PSpice Model available for this device? If not are there any recommendations for trying to simulate this device in PSpice?
Hi Raj kumar Chaurasiya,
Do you want a cross for that part and the FAN one you mentioned earlier? For this device, the best option seems to be UCC21220A . This device is a dual-channel isolated driver. The UCC27324 is a dual channel non-isolated driver…
Hi Robin,
TIDA-00173 does use a clever cascode topology for switching very large voltages, but with a unipolar DC bus. With a bipolar AC waveform, this kind of cascode topology does not work very well, since the current into the zener diode gate clamp…