Part Number: UCC21222 I have one more question regarding UCC21222 .
I need two independent low-side gate drivers to drive two MOSFETs. Does UCC21222 support this configuration?
From the datasheet, I understand that it can be used as a dual low-side…
Part Number: UCC21222-Q1 Other Parts Discussed in Thread: UCC21222
Hello everyone,
I am encountering difficulties with my simulation results after calculating parameters for a GaN ( igld65r055d2.pdf ) driver circuit using the UCC21222 gate driver…
Part Number: UCC21222 Other Parts Discussed in Thread: , UCC21330-Q1 , UCC21330 1. System Specifications:
Power Switch: IGLD65R055D2 (Infineon CoolGaN 600V, 55 mOhm)
Topology: 3-Phase Inverter
Power Rating: 3 kW
DC Bus Voltage…
Part Number: UCC21222-Q1 Other Parts Discussed in Thread: UCC21222 , UCC21551 Hello everyone, I'm having some trouble starting the simulation and would like to ask a few questions below:
1. System Specifications:
Gate Driver: UCC21222-Q1 (TI Model…
Part Number: UCC21222-Q1 Tool/software: Dear Team,
In a back-to-back common drain configuration for a BMS application, I am getting a floating voltage when I turn off the enable signal. What should I do to not get a floating voltage on the output side…
Part Number: UCC21222-Q1 Dear,
Please, could you provide me difference between these two MPNs
SN21222QDRQ1 and SNA21222QDRQ1
Is there any difference between UCC21222QDRQ1 and SN21222QDRQ1?
Thanks in advance for support.
Part Number: UCC21222-Q1 Other Parts Discussed in Thread: UCC21222 , UCC21330 , PMP40500
Tool/software:
Dear TI Team, We are planning to use UCC21222 for our application, could you please confirm UCC21222 is suitable for our system and below are the…
Part Number: UCC21222 My customer is evaluating on UCC21222. Overshoot will happen when output is open loaded and loaded. The deadtime is set up to 100ns from hardware and in software added 500ns as well. The switching frequency is 40kHz.in schematic…
Part Number: UCC21222 Tool/software: Each UCC21222D chip drives the half-bridge consisting of P-channel (high side) and N-channel (low side) MOSFETs. Unfortunately due to a problem in the logic, sometimes we get simultaneous positive pulses on both inputs…
Part Number: UCC21222-Q1 Tool/software: Hi team,
when the VCCI=3.3V, no external resistor/circuit on DIS pin, why the voltage on DIS pin is 2.5V, not 3.3V? beside of the 90Kohm pull up resistor, is there any pull down resistor inside of DIS pin?