Part Number: UCC21320-Q1 Other Parts Discussed in Thread: UCC21550-Q1 Tool/software: Hi team,
For this device, our customer need cover ICT test ,when unpowered up , they will inject a external voltage into UCC21320 VDDA& VDDB pin, they found that…
Part Number: UCC21320-Q1 Hi team,
Could you help check what issue caused the situation? why does high output delay around 2us then turn to low? thanks
Green is High side input
Red is High side output
Blue is low side input
Yellow is low side…
Part Number: UCC21320-Q1 Hello Team, We are designing an isolated MOSFET driver using the IC UCC21320-Q1. The Pin VDDA is driven from an isolated power supply 15V_VDDA and is referring to the GND. The US_ is another voltage that is completely isolated…
Part Number: UCC21320-Q1 Hi team,
May I use UCC21320-Q1 to replace AduM422? but the package is a little bit different.
Any attention will be noted? thanks!
Part Number: UCC21320-Q1 Other Parts Discussed in Thread: UCC21551 Hi team,
If VDDA is below UVLO, but VDDB is OK, will only OUTA be held low while OUTB continiouly follow the input signal (and vise versa)?
Regards, Ochi
Part Number: UCC21320-Q1 Hello,
I am planning to use UCC21320-Q1 to drive 4 pole BLDC Motors.
I would like to know can Channel A source current to the coil when turned on then sink away the current when turned off ? or do I need to use both channel…
Part Number: UCC21320-Q1 Hi team,
Has UCC21320-Q1 passed "VDE V 0884- 11" or just pending? "6.6 Insulation Specifications" looks UCC21320-Q1 follows this certification but "6.7 Safety-Related Certifications" says all certification is still "Planned…
Part Number: UCC21320-Q1
Hi TI team,
May I know how does TI calculate the Supply Current for VDDA and VDDB of typical 2.5mA as shown below?
I am interested to know how the parameters of freq 500KHz, Cout 100pF and VDDA = VDDB = 12V were used to…
Part Number: UCC21320-Q1 Other Parts Discussed in Thread: UCC21530
I have used the UCC21530 a couple of times before and have been very pleased with it, but for a new application channel B is running from a simple 15V supply rail, while channel A bootstrapped…