Part Number: UCC21330-Q1
Hi Expert,
My customer need to do some evaluations for OUT PIN voltage in 12V system when the Drain and Gate of MOSFET are shorted, which means that a 12V voltage is connected with a Rg as below, please help with it, thanks…
Part Number: UCC21330-Q1 Other Parts Discussed in Thread: UCC21330 Tool/software: Hello Team,
Kindly provide the un-encrypted PSPICE model of UCC21330AQDRQ1 IC. This is for my simulation purpose.
Regards
Arun KR
Part Number: UCC21330-Q1 Tool/software:
The customer are using UCC21330Q1 in 800V HVAC compressor.
UCC21330Q1 are used as half bridge driver as the below picture shows.
They find that VDDB are easily to damaged, then VDD PIN is shorted to VSSB.…
Part Number: UCC21330-Q1 Other Parts Discussed in Thread: UCC21330 , UCC5350 , UCC21550 Tool/software:
The customer is using SiC MOS with Kelvin PIN like the below picture shows.
For the E2 pin, whether we have recommendation circuit?
Part Number: UCC21330-Q1 Tool/software: Is the maximum sink/source current specification for the output driver stage (6A/-4A) an internally limited current value? Or is it a warning to the designer to ensure that these current values are not exceeded…
Part Number: UCC21330-Q1 Other Parts Discussed in Thread: UCC21330 Tool/software: Hi, Team,
Do we have replacement recommendation for Infineon 2EDB8259K? This is dual-channel and package is LGA 5x5. Our UCC21330-Q1 is 9.9x6, larger than competitor.…
Part Number: UCC21330-Q1 Tool/software: Hi experts,
The customer want to connect channel A to the bottom bridge and connect channel B to the up bridge because the layout limitation.
So whether it is availiable?
Is there any potential risk?
Part Number: UCC21330-Q1 Other Parts Discussed in Thread: UCC21330 Tool/software: Whether UCC21330 can be used as non-isolated driver?
Which means VSS is connected with GND.
A Channel VDD is 12V compared with SW pin.
B channel VDD is 12V compared…