Part Number: UCC21330-Q1 Other Parts Discussed in Thread: UCC21540-Q1 , UCC21222-Q1 , UCC21520-Q1 , , UCC21530-Q1 Tool/software: Can someone please share the reference design for driving high side MOSFET's with Isolated gate drivers in BMS application…
Part Number: UCC21222 Other Parts Discussed in Thread: UCC21551 , , UCC21530 , SN6501
Hello, the datasheet of UCC21222D does not mention the recommended range of a deadtime resistor.
Assuming that a capacitor ( 2.2nF) to bypass the deadtime resistor…
Part Number: UCC5880-Q1 Other Parts Discussed in Thread: UCC21750-Q1 , UCC5350-Q1 , UCC21530-Q1 Tool/software: Hello,
Multilevel inverters / converters have high no. of MOSFETs / IGBTs. To save PCB space & cost are there any specific MOSFET / IGBT gate…
Hello SY Yoon,
The deadtime programmed in the F280039C device's EPWM module and UCC21530-Q1 are independent. Your timing calculations are correct and the PWM outputs will have a deadband equal to the larger of the two values. So, in this case, the actual…
Part Number: TIDA-01605 Other Parts Discussed in Thread: TIDA-01604 , , UCC21530 , UCC21530-Q1
I have a question about the TIDA-01605 circuit going into TIDA-01604. Currently I am using UCC21530 In the circuit, R30 and R32 were soldered, and R31 was…
Part Number: UCC21225A Other Parts Discussed in Thread: UCC21530 , UCC21540 Hi,
According to Datasheet of UCC21225A, the internal functional isolation between the two secondary side drivers allows working voltage up to 700-VDC.
And the distance of…
Part Number: UCC21520EVM-286 Other Parts Discussed in Thread: UCC21530EVM-286 , UCC20520 , UCC21521 , UCC21520 , UCC21530 Anyone can help to resolve a confusion about the schematic model of this part number which is not reflected properly at the link…
Hi Mukund,
Thank you for your question. I work on the applications team in the high power drivers group.
Your design is using a ground reference supply for your high side driver. This is likely what’s causing your issues. The high side tends to be…
Other Parts Discussed in Thread: UCC21710 , UCC21530 Hi,
Good Day. Customer is working on a fast-acting active clamp for an AC/DC converter where they need an isolated gate driver with low propagation delay (tpd < 50ns) and can drive SiC MOSFETs with…
Part Number: TIDA-010054 Other Parts Discussed in Thread: TMS320F280025C , UCC21530 Hi all,
We are working on a 1kW Dual-Active Bridge Converter. During closed-loop single phase shift voltage control, the lower side MOSFET of the first leg on the secondary…