Part Number: UCC21530 Hello,
1. We are looking for part with Dead time feature of around 400nsec, Shoot through protection.
What is the max dead time setting can be done with UCC21530 IC?
Some datasheets we can see dead time with respect to resistor…
Part Number: UCC21530 Other Parts Discussed in Thread: UCC21551 There's only one gate driver of UCC21530 used. it means the other one gate drive is unused and needs to disable.
How to deal with unused INx pin VCCx and OUTx pin?
If unused gate driver…
Part Number: UCC21530-Q1 Other Parts Discussed in Thread: UCC21551 The VCC and the Enable PIN are provided with 5v. Please find the picture below. Why the enable pin shows less voltage of around 2.6V? Is there any reason for this?
Please find the picture…
Part Number: UCC21530 Customer is asking for a test result of the Mechanical Stress Test for the device strength during mounting and assembly proccessing.
Not sure if the standard is referring to " J-STD-002" or not? Could you kindly help to offer…
Part Number: UCC21530-Q1 Other Parts Discussed in Thread: UCC21530 hi
TI friends about UCC21530-Q1 the folowing questions pls help
1.my customer wanted to know the 5700V of UCC21530 was effective valu e or peak value ,
2. if it is safe for it when we give…
Part Number: UCC28951 Other Parts Discussed in Thread: UCC21530 , , UCC27525 What is the maximum voltage level of OUTA-OUTF? Assuming it is same as VDD(12V).
As the reference SCH shown, the power supply of UCC21530 VCCi is 5V. and Datasheet of UCC21530 does…
Part Number: UCC21530-Q1
As you can see that there are two waveform in the oscilloscope. Top one is the output of the gate driver first channel output OUTA (yellow in color) and the below one is the driver input given from the STM microcontroller ( blue…
Part Number: UCC21530-Q1 Other Parts Discussed in Thread: UCC21530 Hi team:
The UCC21530-Q1 was failed On our customer side.We have below questions which our customer is also concerned about.
We need to confirm the peak current value which is allowed…