Part Number: UCC21222-Q1 Other Parts Discussed in Thread: UCC21540-Q1 , UCC21520-Q1 Hi team,
How much channel to channel voltage could UCC21222-Q1 deal with? Another device, such as UCC21540-Q1, shows its "Channel to channel isolation voltage" abs max…
Part Number: UCC21222-Q1 Other Parts Discussed in Thread: UCC21540-Q1 , , UCC21520-Q1 , UCC20225-Q1
Hey Team,
I have a customer that is deciding between the UCC21222-Q1, UCC21520-Q1, and UCC21540-Q1 for a Belt Start Generator (BSG) automotive application. …
Hi, Gabriel,
I would recommend UCC21540-Q1 if a dual driver is required. Since we don't have a dual-driver with Miller Clamp, you will need to use the split-supply to help. There are several examples of split-supply in the datasheet.
Part Number: UCC21736-Q1 Other Parts Discussed in Thread: LMG1210 , LMG1205HBEVM , UCC21540A , LMG1205 , UCC21540 Hi,
I have an application where I need to drive a Silicon MOSFET (Part number: SISS08DN-T1-GE3; Datasheet: https://www.vishay.com/docs/76780…
Part Number: UCC5870-Q1 Other Parts Discussed in Thread: UCC21750 , ISO5851 , UCC21710 , UCC21540 Hello everyone,
I am building a grid connected system, which consists of a three phase inverter (2 level AFE) and two parallel DC-DC converter (LC-SRC) which…
Hi Sébastien,
Yes, this could potentially work. In the orderable part number UCC21540AQDWKRQ1:
“A” denotes a version. This part is UCC21540A and has 5-V UVLO (different from UCC21540 which has 8-V UVLO). See the datasheet table included below…
Other Parts Discussed in Thread: UCC21540-Q1 , SN6505B Hi
Lets assume that i am building a fullbridge/H-bridge and that i am for instance using LMG341xR070 or UCC21540-Q1 to do so.
To power the high side of the H-bridge i want to power from an isolated module…
Part Number: UCC21540A-Q1 Other Parts Discussed in Thread: UCC21540 I am trying to simulate the driver circuit using UCC21540 IC. I am getting the following message in LTSpice and the errors are due to the UCC21540 model. The simulation is going on forever…
Part Number: UCC21520-Q1 Other Parts Discussed in Thread: UCC21530 , UCC21520 , UCC21540 Hi,
My customer's application is in 800V bus voltage application. They chose the UCC21530 in before, but met the noise issue for the low UVLO threshold. So they change…