Part Number: UCC21540A Hi, We seem to have a layout issue with the UCC21540A on an interleaved boost circuit. We are certain the circuit works well because we have versions of it that do not have this problem. The logic side is 5V powered and each output…
Part Number: UCC21540A Other Parts Discussed in Thread: UCC21540 Dear sir,
would you please check whether UCC21540ADWKR can meet the following latest safety qualification, if so, do me a favor to provide the certificate:
VDE-0884-11
62368-2020
60747…
Part Number: UCC21540A-Q1 Other Parts Discussed in Thread: UCC21540 I am trying to simulate the driver circuit using UCC21540 IC. I am getting the following message in LTSpice and the errors are due to the UCC21540 model. The simulation is going on forever…
Part Number: UCC21540A-Q1 Hi Expert,
Do we have comparing table for NCV57252? Could you please help recommend a better performance device competing NCV57252? Thanks.
BR,
Elec Cheng
Part Number: UCC21540A-Q1 Hi sir, We are planning to use UCC21540AQDWKRQ1 driver IC to drive high side and low side FETs in the same leg of a 3 phase inverter in motor drive application. Since there are 3 such legs we are planning to use 3 such driver ICs…
Part Number: UCC21540A-Q1 Hi TI,
Given that UCC21540A-Q1 has a UVLO rising threshold max of 5.9V, which accords with the minimum recommended VDD of 6V, is UCC21540A-Q1 suitable for driving GaNFETs with 6V absolute max V_GS?
Suppose that an ideal 6.5V…
Part Number: UCC21540A Other Parts Discussed in Thread: UCC21540 , Hi TI expert
In the >More literature link there is the GB4943.1-2011 certificate that I found, but I couldn't find one for UL 1577. In the datasheet for UCC21540ADWKR it states certifications…
Part Number: UCC21540A Other Parts Discussed in Thread: UCC21540 Hi,
I am working on a 3 phase motor control project and use UCC21540 isolated gate driver to drive my IGBT. Does the UCC21540 driver work with our supply from -170 to 170VDC? If it does not…
Part Number: UCC21540A Hi Team, Our customer is looking for the footprint/schematic symbol for UCC21540A to be imported in Altium. Can you provide us the bxl file for this device? Thanks in advance! Kind Regards, Jejomar