Part Number: UCC21551-Q1 Other Parts Discussed in Thread: UCC21551CQEVM-079 Hello,
We are planning to use the UCC21551x isolated gate driver in a motor drive application.
In the datasheet/layout guideline, the following recommendation is given:
…
Dear Amy,
Thank you for your support.
2. About enable pin, I saw that 90kohm pulldown is attached internally in block diagram. Is internal pullup in your answer typo?
(1) As I said, nFAULT_OCP_IN is from current sensor's output. Current sensor…
Part Number: UCC21551-Q1 Hello TI team,
Can the UCC21551-Q1 DFJ package be used in a 1500 VDC system?
The channel-to-channel rating is 1850 VDC, but the distance between the two channels is only about 5.3 mm. My understanding is that at least 8 mm…
Part Number: UCC21551 Hi,
I'm designing a traction inverter and want to implement ASC (Active Short Circuit) protection.
Background:
Some driver have built-in ASC protection
I'm using UCC21551 (no ASC input)
I need to implement ASC protection…
Part Number: UCC21551 Other Parts Discussed in Thread: UCC21530 Hi Ti Team,
For my totem-pole PFC design I am using the isolated dual gate driver UCC21551 from TI to drive SiC MOSFETs. For SiC devices, a small negative gate bias during turn-off is usually…
Part Number: UCC21551 Other Parts Discussed in Thread: UCC27212 Hi all,
I previously opened a thread with the same title, but it seems to have been removed, so I am reposting my question here.
I am working on a high-side power switch design using…
Part Number: UCC21551 Hi TI Team,
I'm using UCC21551BDWKR to drive 8 parallel MOSFETs per switch position (16 total per phase leg) in a motor controller.
22R gate resistor per MOSFET
Switching frequency: 8-15kHz
Bus voltage: up to 96V
Is…
Part Number: UCC21551-Q1
Hello TI Team,
The UCC21551-Q1 datasheet specifies a channel-to-channel creepage distance of >5.3 mm for the DFJ28 package and >3.3 mm for the DWK package. However, the Absolute Maximum Ratings specify the same channel-to…
Part Number: UCC21551 Other Parts Discussed in Thread: UCC21520 Tool/software: Hello, I'm Cheol-ha kang.
I am a hardware engineer based in South Korea, specializing in the development of converters for the automotive industry.
First, before I ask…