Part Number: UCC21710 Hello ,
We are facing a wierd issue with out NTC temperature circuit.
When ever the MOSFET is switching we seem to be getting an accurate reading , but the moment the mosfet stops switching we see an offset being added to the…
Part Number: UCC21710-Q1 Other Parts Discussed in Thread: UCC21710 Tool/software: What is the typical required, recommended schematic and good layout practice for UCC21710Q1 and UCC21710
Part Number: UCC21710-Q1 Other Parts Discussed in Thread: UCC21710 Hello,
I'm using UCC21710 and would like to utilize OC pin for overcurrent protection.
Since I have a current sensor on the low voltage side, I am using a digital isolator to transmit…
Part Number: UCC21710
Tool/software:
Hello Experts,
We are designing the OC threshold limits and a little confused as to that limits we are allowed to set.
Firstly the SiC module we are using is the MSCSM120HM16CTBL3NG
Looking at the datasheet…
Part Number: UCC21710 Hello, we are using the UCC21710 (and UCC21737, but basically it should be the same for this question) with very small resistors for turning on and off - around 0.1 to 0.4 Ohm. As the internal turn on and turn off MOSFETs are given…
Part Number: UCC21710 Tool/software: Hello Team,
I am having one query.related to voltage levels of PWM lines on UCC21710.
I am providing 5V VCC supply on pin no 15 of UCC21710. but my microcontroller output voltage.is 3.3V.
So my PWM voltage levels…
Part Number: UCC21710 I am using UCC21710 to drive 2 SiC MOSFETs in parallel. Based on the discussion in another link of e2e ( https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system…
Part Number: UCC14241-Q1 Other Parts Discussed in Thread: UCC21710 Tool/software: Hi,
I am trying to use the UCC14241 integrated power supply along with the UCC21710 isolated gate driver for driving SiC MOSFETs. The desired voltage rails are +16V (Vdd…
Part Number: UCC21710-Q1 Other Parts Discussed in Thread: UCC21710 Tool/software: Hi,
I am finishing a gate driver design using the UCC21710 gate driver IC for SiC MOSFETs.
I have been using the SLUC695 calculator tool to check my design and additional…
Part Number: UCC21710-Q1 Tool/software: Hello.
I would like to confirm the Vocth of the OC pin.
Vocth (Detection Threshold) is specified as follows on the data sheet.
Vcoth min 0.63V - max 0.77V
However, when I measured at -20C, it was 0.61…