Part Number: UCC21750-Q1
Tool/software:
Hi~
I have a few questions.
1. When I designed and measured the Desat circuit as shown below, it worked as shown in the measured waveform. Please check if it is working normally.
2. If the desat setting…
Part Number: UCC21750 Tool/software: Hi Team, We need you support on selection of preferred current amplifier / driver part number for UCC21750QDWQ1. which is having 10A peak current. But out requirement is 20A. We wanted to used same Gate Driver along…
Part Number: UCC21750-Q1 Tool/software: Hi~
The guideline states to apply a Bead to the FET Gate as follows ( file name : UCC217xx Schematic and Layout Design Guidelines_RevA.xlsx)
If a bead is added, its purpose should not be to control noise from…
Part Number: UCC21750
Tool/software:
Hello Experts We are just designing an MPPT with 400Vdc and 800Vout. However, how to calculate turn-on gate resistance (Rg_on) and turn-off gate resistance (Rg_off) in the UCC21750 gate driver for SiC Mosfet-based…
Part Number: UCC21750-Q1 Other Parts Discussed in Thread: UCC21755-Q1 , Tool/software: UCC21750-Q1 seems to be getting discontinued. The web recommends UCC21755-Q1 as a drop-in replacement. Is there any difference between the 2 at all? I had a quick look…
Part Number: UCC21750 Tool/software: Hi Team,
Could you please help share more materials about DESAT function? Customer is concern the performance because when they do short-circuit test, IGBT will damage 10 times test.
BRs,
Francis
Part Number: UCC21750 Other Parts Discussed in Thread: TXS0108E-Q1 Tool/software: Hello,
We are now using UCC21750 for driving. Primary side we use 5V power supply, and all the signal pins (IN+, IN-, RDY, FLT, RST) are driven by voltage level chip TXS0108E…
Part Number: UCC21750-Q1 Other Parts Discussed in Thread: UCC21750 Tool/software: I'm troubleshooting a half bridge module that uses two UCC21750s. After a few minutes under load, the low side IC will assert the fault pin, stopping operation. On the control…
Part Number: UCC21750-Q1 Other Parts Discussed in Thread: UCC21750 Tool/software: Hi~
Please tell me the required current for the gate input terminal of UCC21750-Q1
Part Number: UCC21750-Q1 Other Parts Discussed in Thread: UCC21750
Tool/software:
Hi,
I want to use the UCC21750 with an external totem pole buffer to drive a SiC power module (CAB6R0A23GM4T) at 25kHz. In section 9.2.2.8 of the gate driver IC, the…