Part Number: UCC23513 Other Parts Discussed in Thread: UCC21551 Dear Experts,
I am looking for an IC that has got the same features of UCC23513, but with 2 channels. I am using this IC as an alternative for optocouplers to shift 5V to 15V and provide…
Part Number: UCC23513 We had tested the UCC23513 of the input and output performance. We find the If current have slightly high at turning high, and has slightly ringing at turning off. The turning off ringing also cause the output voltage has the same…
Part Number: UCC23513-Q1 Dear teams,
When I saw the typical application, I found that PWM could control this IC through the MOS (switch).
If I want to simplify it (don't use switch), could I use MCU to control it directly? Or is there any suggestion…
Part Number: UCC23513 Hi Team,
I have asked below UCC23513: questions on power dissipation - Power management forum - Power management - TI E2E support forums
Customer still has more questions
as mentioned
" The recommended max If is 16mA and the absolute…
Part Number: UCC23513 Hello,
I am driving the output of the UCC23513DWY with ±12V from a ±12V power supply TMA 0512D. They are driving the gate of a mosfet IXFN360N, which is where it gets its return back to the power supply common. These are isolate…
Part Number: UCC23513 Hi,
What is the UL number of UCC23513DWYR? Is it number for 20190711-E181974 on the attached file?
Please help to confirm it. Thanks!
sluq004-ucc23513.pdf
Part Number: UCC23513 Hi expert team
Our customer wants to access the reliability of UCC23513, I know we have MTBF/FIT estimator on TI.COM, but customer wonders that if we have some calculation to do more detailed analysis, for example, an excel with…