Part Number: UCC24612-1EVM Other Parts Discussed in Thread: UCC24612 , LM5026 , UCC24610 Hi
My customer used LM5026 and put the UCC24612 EVM in the secondary low-side MOSFET.
The CH1(Yellow) is EVM's gate. Is there a need to modify it?
Thanks…
Part Number: UCC24612-1EVM Other Parts Discussed in Thread: UCC28780 , UCC24612
Hello,
Is it possible for you to send the gerber file of UCC24612-1EVM?
I also want to create footprint for other mosfets if you send me the Altium project…
Part Number: UCC24612-1EVM Other Parts Discussed in Thread: UCC24612 , Hello,
What changes would you recommend to the application circuit for 12VOUT application at 5A?
Do you have any recommendations on Si MOSFET p/n?
Part Number: UCC24612-1EVM Other Parts Discussed in Thread: UCC24612 , Hello,
I am using the UCC24612-1DBVR in a POE supply. This power supply, a TI-design (TIDU190-January 2014), has a 12V 15W fly-back topology.
In the DCM mode (Discontinuous Conduction…
Part Number: UCC24612 Hi Team
Currently using 24612 on the new board, there is a problem: Gate cannot be opened normally as shown in the figure below (load0.5A-5A cannot be used) Using UCC24612-1EVM on customer board can be opened normally, but after…
Part Number: TPS23753A Other Parts Discussed in Thread: UCC28780EVM-002 , UCC24612-1EVM Hello Expert,
Our customer has thermal issue on their b'd and they are using tps23753a.
Their application is IP Network Camera.
The heavy thermal points are…
Part Number: UCC25630-1EVM-291 Other Parts Discussed in Thread: UCC24612-1EVM , CSD18536KCS , CSD18535KCS , UCC24612 Hi all,
UCC25630-1EVM-291 is full wave two Diodes Rect.
Many customer want to change Diodes to SRs.
But UCC24612-1EVM is expensive…
Part Number: UCC24612 Other Parts Discussed in Thread: LM358B
We are attempting to use 24612 for converting our existing DC-DC converter with flyback topology from diode rectification to synchronous rectification. Models are 12V 2.5A or 5V 6A. At present…
Part Number: UCC256303 Other Parts Discussed in Thread: UCC25630-1EVM-291 Dear colleague,
The customer has encountered the below issue:
1. Now they have a UCC256303 for a project. Now there is a problem with the startup. When starting, the resonant…
Part Number: UCC24612 Other Parts Discussed in Thread: UCC24630 , UCC24610 Hi,
I am designing a SEPIC SMPS with an output current of 10A. Given the output current, I'm considering the use of a synchronous rectifier controller to replace the output diode…