Part Number: UCC24624 Hello,
We would like some help understanding the markins on the UCC24624 chips in the pictures. Can someone tell us the difference between the two parts? What are the manufacturing locations, date codes, and any issues with the…
Part Number: UCC24624 Hi,
I want to design an LLC resonant converter with a half-bridge rectifier, with a maximum output voltage of 105V and a maximum output power of 12kW. The Drain-Source voltage of the switches in the half-bridge rectifier is 210V…
Part Number: UCC24624 Other Parts Discussed in Thread: UCC256403 Tool/software: We have designed one 750W EV charger for electric 2 wheeler. The output voltage & current are 58 V,12 A. The DC-DC stage is an half bridge LLC resonant converter. I have attached…
Part Number: UCC24624 Tool/software: Hi Experts,
My customer is evaluating UCC24624 in an industry power module:
Secondary voltage: 70V
Secondary RMS current: 330A
Switching Frequency: 30K-100KHz
Since the power rating is high. We need to…
Part Number: UCC24624
Hi,
Our customer, Rubycon, is considering the UCC24624 for synchronous rectification in a 24-V output LLC application.
Under an output overvoltage condition, the voltage applied to the UCC24624 VDD…
Part Number: UCC24624 Other Parts Discussed in Thread: UCC24610 , LM5026 Tool/software: Dear Sir,
Can we use UCC24624 in active clamp forward converter to drive SR mosfets. Because in the datasheet it is mention that UCC24624 is dedicated for LLC resonant…
Part Number: UCC25600-DESIGN-CALC Hello,
I am attempting to simulate an ac/dc design and would like to run a sim of the LLC / RC stage with these two parts however the models don't run in simetrix elements - please could I get uynencrypted models…
Part Number: UCC24624 Tool/software: The input transformer is fed with an AC signal of 264V at 30kHz +/- 12kHz ( NOT LLC). Previously we were using half bridge diode rectification to get the output voltage of 48V.Now We want to modify the circuit having…
Part Number: UCC24624 Tool/software: Hello
I have an LLC DC-DC design with output voltage at 48V and I need to add synchronous rectification controller at the seconder side. I found UCC24624 IC and seems like ok for my design.However as mentioned in…