Part Number: UCC25600 Other Parts Discussed in Thread: UCC21520 Hi All,
I am using isolated DCDC converter with LLC topology, where primary side has full bridge & secondary diode bridge.
I am thinking to use UCC25600 as controller for this LLC.
I…
Part Number: UCC25600 Hi team,
Customer has an issue
I'm looking to design a Resonant half bridge converter using the UCC25600 controller. Most of the parts are selected, outside of the feedback system. I have seen a prior thread mentioning issues with…
Part Number: UCC25600 Other Parts Discussed in Thread: UCC256403 The frequency at which burst mode occurs, is 350kHz.
Can this be lowered to 240kHz, as an example?
(Burst mode will only happen at no-load to prevent the output voltage from running away…
Part Number: UCC25600 The specs of this design are:
Input Voltage: 39V to 60V (nominal 48V)
Output Voltage: adjustable from 39V to 60V (nominal 48V)
Output Power: 500W
Using the design guide slups63.pdf to design the rssonant tank of a half bridge LLC…
Part Number: UCC25600 Other Parts Discussed in Thread: UCD3138 , Hi,
My customer wants to use UCC25600 to study the full bridge LLC. And they do not use UCD3138 or C2000.
Does TI have any information about the application of UCC25600 in full bridge LLC…
Part Number: UCC25600 I need design dc to dc converter , I need 2.5kw , vout: 24~36V I will want use ucc25600 full bridge Do you have any related designs for reference
Part Number: UCC25600-DESIGN-CALC Other Parts Discussed in Thread: UCC25600 Hi
We are designing LLC resonant converter using UCC25600. if there is already existing mathcad file please share with us.
Regards
Nitesh Kr Jha