Part Number: UCC256301
Tool/software:
Hi buddy Ive been trying to find SLUP263 (LLC Design docs) on your website but I couldn't find it. Is there any problem? With Best Regard Kasra Latifi Frad Kasra.Latifi-Fard@tdk.com
Part Number: UCC256301 Other Parts Discussed in Thread: TIDA-010015 Hello Sir/Ma'am,
I'm trying to implement the reference design of TIDA-010015 through PSpice for TI software. But meanwhile I'm facing problem with placing of UCC256301…
Part Number: UCC256301 When UCC256301 stops and the output voltage drops slightly below the set voltage, when UCC256301 restarts, the output voltage will jump.
It is set to output 24V, but the output jumps to 28V.
There is a period of 14ms in which switching…
Part Number: UCC256301 Hello All , Manikanta,
May i ask you to help with FA analysis of few samples of Part • UCC256301LLC controller SOIC16 from TEXAS INSTRUMENTS.
Since we using it in mass production and periodically faced with issues
Thank you in…
Part Number: UCC256301 Other Parts Discussed in Thread: UCC25600 I need to design a 500w 50V max power supply with the possibility of varying the out voltage on three levels, 17, 34, 50V to drive a resistive load with different powers and currents
Is it…
Part Number: UCC256301
I need a pure sine, soft-switched resonant constant-voltage DC/AC inverter, operating at 100 kHz, up to 20A @ 5V.
The load is inductive: several parallel coupled-inductors for galvanic isolation.
There should be a simple feedback…
Part Number: UCC256301 Other Parts Discussed in Thread: UCC28950 Hello TI wizards!
I have a requirement for an isolated DC-DC converter with an input of 350VDC to 400VDC and an output of 380VDC at 8A max. Is this something the UCC25630-1 could handle?…
Part Number: UCC256301 Other Parts Discussed in Thread: UCC256302 , UCC256402 Hi Team!
I have questions about the LL value in the simplis model.
Is that a voltage value or something else?
What does it represent and how does it affect the simulation?
…
Part Number: UCC256402 Other Parts Discussed in Thread: UCC256301 , UCC25640
Hello,
My customer Nestle needs to switch from the UCC256301 to the UCC256402 due to delivery issues.
They tested the '6402 in their exisitng design and observed higher temperature…
Part Number: UCC256301 Other Parts Discussed in Thread: UCC256402 Hi Team,
My customer is using UCC25630-1DDBR as the controller of an LLC converter they designed. Although the outputs of the converter are as expected, the temperature of UCC25630-1DDBR…