Part Number: UCC2580-1 Dear all,
one of my AA is using the UCC2580-1 in avionic application. The device works fine, according to the MIL-704 which considers only fast ramp on the Input voltage supply and so on VDD.
The designers are tryng to qualify…
Hello Mark,
These signals are completely independent.
REF is a nominal 5V reference voltage with 2.5% tolerance
LINE is used to enable the UCC2580-1 when the input to the pin is 5v (6% tolerance) on a rising LINE signal.
LINE is used to disable a…