Part Number: LM5035 Other Parts Discussed in Thread: UCC25800 Hi team,
Here is an application that we are reaching to you here.
My ctm is wanting to use LM5035 as a open-loop controller for a 50% duty cycle half bridge LLC such as our UCC25800 for…
Part Number: UCC27282-Q1 Other Parts Discussed in Thread: UCC25800 , UCC27212 , TLV1805 Hello - We are using this part already for a motor driver circuit but are considering repurposing it as a battery distribution switch in another circuit. We only need…
Part Number: UCC5390 Other Parts Discussed in Thread: SN6505B , UCC14240-Q1 , UCC25800 Customer is using UCC5390ECD as an isolated drive for high side FET switch.
Can confirm whether it can drive 100% duty cycle?
Hello Jonathan,
You're correct - you can use the same VCC1 as the primary side power supply. As of the secondary side power supply, the two gate drivers should each get its own set of bias supply, since they are connected to MOSFETs of different source…
Hello Furkan,
The UCC27714 high side driver can operation in a DC operating condition but you are correct that with a bootstrap method for the high side floating bias the DC operation is not possible. You can use a floating high side bias solution such…
Hi Minh,
I would suggest to take a look at any of the UCC217xx family with OC pin. I would suggest to look first at UCC21710 or UCC21732 based on the information youve provided. OC-pin based short circuit detection has timing advantage for SiC FETs…
Part Number: UCC28500 Other Parts Discussed in Thread: UCC25800 Hello,
My customer is using UCC25800 for a Boost + forward converter, the input range is 150V-800V DC, output is 24V. And for boost stage the output is 460V, no PFC function required…