Other Parts Discussed in Thread: UCC27424-Q1 , UCC27200-Q1 , TIDA-00120 Hello,
I would like to know if there is any buck converter and driver in the same package with PWM inputs. I am going to use it with a C2000 piccolo with MPPT algorithm.
Thank you.
Other Parts Discussed in Thread: UCC27200 Can multiple mosfet driver IC's such as the UCC27200/1A be coupled together to drive a single half-bridge? Each UCC will drive a mosfet hi/lo pair but all the switchpoints (HS) will be common.
Other Parts Discussed in Thread: UCC27211 , CSD18532Q5B , UCC27200 Hello all,
I am using Simetrix 7.20f as simulation environment, and want to simulate a circuit containing the UCC27211.
For this part only a encripted SPICE model and Tina models are available…
Other Parts Discussed in Thread: UCC27200 , UCC27201 can anybody suggest me what should be the Mosfet and mosfet driver if i want to design Stepper Motor Driver of 100V & more than 5A Stepper motor?
Dears,
I am looking for a high side and low side driver to replace LTC4444-5.
VCC is required down to 5V and input PWM frequency is 120KHz. So UCC27200 or LM5101 also do not match due to the higher VCC.
I do not find a proper device, can you please…
Other Parts Discussed in Thread: UC3846 , UCC3806 , UCC27200 , LM5045 Can UCC3806 be used for Full Bridge Topology? I initially decided on UC3846 and then found UCC3806 similiar with the later having advantages. While the product page of UC3846 lists Full…
Other Parts Discussed in Thread: UCC27201 , UCC27211 , UCC27210 , UCC27200 Any plans to qualify the UCC27210 and UCC27211 to AEC-Q100? These are based on and include performance improvements over the UCC27200 and UCC27201 (which come in a Q1 version).
Other Parts Discussed in Thread: CSD18532Q5B , UCC27200 Can someone please translate the encrypted CSD18532Q5B model to either simplis or a non encrypted spice model? Non encrypted spice model may work depending on the complexity of the model to import into…
Other Parts Discussed in Thread: UCC27211A , UCC27211 , UCC27201 , UCC27200 Hi forum,
I'm working on a BLDC controller and had a look at the UCC27211/UCC27211A gate driver. But I cannot spot the big difference between the non-A version and the A-version…