Part Number: UCC27282-Q1 Other Parts Discussed in Thread: UCC27282 Hi team,
The following figure is my design. The function I want to achieve is to output high-voltage periodic square wave.
The supply is 12V,input is the 5V@11Khz,output is 90V,Theoretically…
Part Number: UCC27282 Other Parts Discussed in Thread: UCC27289 , UCC27288 , , UCC27284
Hi, TI expert
I am looking for a gate driver device, it is photovoltaic application.
I see there are some devices which meet my requirement, some questions:
1. What…
Part Number: UCC27282 I am using UCC27282 Gate drivers to turn on Mosfets in a Half Bridge (using three Gate drivers for three phase inverter). MOSFET part number is IAUS300N10S5N015T . The dead time has been configured to 2 us. As soon as High side PWM is…
Part Number: UCC27282 In UCC27282 datasheet, The delay time of VHI rising to VHO rising is 30ns max,but in my testing ,the dalay time is 174ns,
Channel 2 tested at pin7, and there is no RC delay.
channel3 tested at mosefet Gate-source.
I also check oscilloscope…
Part Number: UCC27282 Hi expert,
My customer is using UCC27282QDRCRQ1 first time and it is for a 300W Sync boost, the two MOSFET are CSD19502.
PWM switching frequency: 60KHz
Duty cycle: 20%(the main switch turn on for 20% time)
They increased the input…
Part Number: UCC27282-Q1 Other Parts Discussed in Thread: UCC27282 , LM317MQ Hi Team,
There is a question here about UCC27282-Q1. Is there any requirements for voltage on Pin1 Vdd? We promote UCC27282-Q1 to alt Diodes DGD05473FNQ. But UCC27282 needs Vdd…
Part Number: UCC27282-Q1 Dear Support,
Good day,
Kindly help me on the part number UCC27282QDRQ1 for the tape and reel information.
Please confirm if it is normal if there is no empty tape at the beginning of the reel?
I cannot find this in tape and reel…
Hello Sherry,
If 3A is not enough, then this driver is not appropriate. There are some techniques to boost drive strength, like the BJT totem-pole shown here:
But it is probably better to just choose a different driver. The older generation part, UC…
Part Number: UCC27282 Other Parts Discussed in Thread: LMG1210 I'm making a class D amplifier with the UCC27282. Can his LI and HI be used as comparators? If not, can you recommend me which comparator can input 15MHz.
Part Number: UCC27282 Other Parts Discussed in Thread: CSD19536KCS
Hello team,
I am writing because I am doing in design of an inverter with the UCC27282 and the CSD19536KCS.
The circuit works fine up to 24Vdc, but, when I try to bring the supply voltage…