Part Number: UCC27282-Q1 Tool/software: Hi HPD experts!
May I know why the HS HB HO HBM are marked lower between and other pins? What makes the difference?
Thanks!
BR
Josh
Part Number: UCC27282-Q1 Other Parts Discussed in Thread: UCC27282 , , LM2105 , LMG1205 Hi team,
Do we have alternatives for UCC27282-Q1 which the VDD can accept 5V? For UCC27282, seems that nomimal is 12V and min is 5.5V.
My customer wants to use 5V in…
Part Number: UCC27282-Q1
Tool/software:
Hello! As it says in the title I've been trying to make an active Sodium-Ion ESP32 active battery balancer using the UCC27282-Q1 for the past couple of months. I came up with 2 different versions, none of which…
Part Number: UCC27282-Q1 Tool/software:
We are using UCC27282QDRQ1. We want to run motor at 72V & 250A current. we are not able to run IC above 48V. Above 48V IC & MOSFET are getting Damaged. I have attached the circuit we are using. Please verify & suggest…
Part Number: UCC27282-Q1 Tool/software: What is the minimum forward voltage drop of the bootstrap diode across different temperatures? The datasheet provides the typical and maximum values, but I need the minimum value to select an appropriate external…
Part Number: UCC27282-Q1 Other Parts Discussed in Thread: UCC27284-Q1 , UCC27311A-Q1 Tool/software: Hi Team,
This is FAE Jayden, My customer would like to know do we have a device which has the same package with UCC27282Q1 but without interlock function…
Part Number: UCC27282-Q1 Tool/software: I have been using slva504a to try and estimate the power dissipation of the FETs in an H-bridge being driven by the UCC27282-Q1 driver chip. I have a spreadsheet, when I use a very small load current like 12 mA…
Part Number: UCC27282-Q1 Other Parts Discussed in Thread: UCC27282 Hi expert,
From datasheet, the UCC27282 is quite fit for BLDC/PMSM motor gate driver, such as interlock protection, negtive voltage protection, integrated bootstrap diode, small package…
Part Number: UCC27282-Q1 I'm encountering a problem where the switch node in my gate driver fails and the reverse bias measurement of the bootstrap diode is not open when the bus voltage is increased to around 45V. I suspect this issue might be due to…