Part Number: UCC27282 Other Parts Discussed in Thread: UCC27289 , UCC27288 , , UCC27284
Hi, TI expert
I am looking for a gate driver device, it is photovoltaic application.
I see there are some devices which meet my requirement, some questions:
1. What…
Part Number: UCC27288 Good afternoon,
I have been struggling for a couple of weeks now implementing the UCC27288DR Gate Driver to drive IPP200N15N3 Mosfets for use in a 3 phase motor driver. The control works and the motor operates successfully, however…
Part Number: UCC27288 Hi All,
I'm looking for a way to calculate or determine the maximum switching frequency based on the information available in the datasheets. Using the UCC27288 as an example, is there a way to use the switching characteristics to…
Part Number: UCC27288
Hello team, I’ve got a question from the customer, and would like to ask your advice.
What would be the benefit for the customers to use half-bridge driver with external bootstrap diode (like UCC27288) ?
Would the external…
Hello Yun,
As Richard mentioned, there are several 600V half-bridge drivers that do not have the integrated diode from TI. Here are a couple of the 100V half-bridge drivers we have available at TI: UCC27288 and LM5109B-Q1.
Best,
Avery
Hi Ben,
Thank you for reaching out! It sounds like you will want to implement charge pump circuitry to help keep the boot cap charged. TI has a tech article available that helps explain the process for implementing a charge pump: Link . I am unaware of…
Hello Richard, really thanks.
Ok UCC27288 for my application so I can design the boot diode.
About DC BULK Capacitor (or called also DC-Link Capacitor), could you tell me if you have a guidelines or application notes to properly size this capacitor given…
Part Number: UCC27211A Other Parts Discussed in Thread: CSD19536KTT , UCC27211 , UCC27288 , , UCC27289 Dear,
I am designing a BLDC Motor stage with UCC27211 as gate driver and CSD19536KTT mosfet. Power supply of motor is 48 Volts.
My schematic is as follow…
Hi Damian,
It is not recommended to have large difference in voltage between the device and h-bridge. I suggest looking into the UCC27288 half-bridge high voltage driver as an alternative solution to using the DRV8701. The UCC27288 does not have OCP which…
Part Number: UCC27524 Other Parts Discussed in Thread: UCC27288 , UCC27282 , UCC27284 Dear Team,
Here is Kevin from Delta Taiwan.
Customer is looking for TI device to replace IR2085STRPBF
infineon.com/dgdl/Infineon-IR2085S-DS-v01_02-EN.pdf?fileId=5546d46…