Part Number: UCC27289 Hi all,
Is it possible to use a pair of UCC27289 to drive an external h-bridge for brushed motor?
Is there an example scheme or an application note that shows the configuration?
Regards,
Lorenzo
Part Number: UCC27289 Other Parts Discussed in Thread: AFE5832 , LM3488 , TX7332 , TIDA-010057 , Hello TI experts,
Last time I asked about LM3488, for operating 4 x TX7332 and 2 x AFE5832 based on TIDA-010057.
https://e2e.ti.com/support/power-management…
Part Number: UCC27211 Other Parts Discussed in Thread: UCC27288 , , UCC27289 , UCC27284-Q1 , LM25145 , UCC27624 , UCC27614
Tool/software:
I am designing a full H-bridge circuit with an output voltage (V_DS) of +1.6V and an output current ranging from…
Part Number: UCC27321 Other Parts Discussed in Thread: UCC27289 , UCC27284 , UCC27212A-Q1 Hi team,
Does TI have same spec or better of pin driver solution? Competitor: EL7155CSZ-T7
Part Number: UCC27211 Other Parts Discussed in Thread: UCC27289 Hi,
I'm looking for replacement part with enable/disable function for UCC27211. If you have any suggested part, please let me know.
Thanks!
Part Number: LM5100A Other Parts Discussed in Thread: UCC21540 , , UCC25600 , UCC27289 , UCC21520 , UCC21530 Tool/software:
To whom it may concern
We want to use UCC25600, but we have a problem in design because of LM5100A which is the gate driver…
Part Number: SM72295 Other Parts Discussed in Thread: UCC27301A-Q1 , UCC27289 , UCC27211A , UCC27201A , UCC27282 , UCC27284 , UCC27311A-Q1 , BQ2031
Is it possible to use this part in a single half-bridge configuration i.e. the 'A' side to implement…
Hello Chase,
For high frequency operation, I would recommend the UCC27289 over the UCC27211A. This is mainly due to the improved narrow pulse performance and lower propagation delays in the UCC27289 compared to the UCC27211A.
I did confirm with quick…
Part Number: LM25101 Other Parts Discussed in Thread: UCC27289 , SN6501 Hi,
We found there is about 6V on HS when LM25101 is used to driver the high-side and the low-side N-Channel MOSFETs in a synchronous buck. The VDD is 10V.
It can be p ulled down…
Other Parts Discussed in Thread: UCC27289 Intro
Typically, most ICs are available in industry standard packages such as SOIC and DFN. Even among competitors, many devices are designed to have the same pinout so they can be easily replaced or upgraded…